ADA4622-2: FAQ

  • ADA4622-2 compared to AD822

    Question What are the benefits of using the ADA4622-2 compared to the AD822? Answer The ADA4622-2 includes many improvements that make it desirable as an upgrade without compromising the flexibility and…
  • Applications of ADA4622-2

    Question What applications is this part aimed at? Answer The ADA4622-2 can be used in many different applications but it’s very low bias current mean it is particularly suited to interfacing with highoutput…
  • Design tools

    Question What tools are available to help me design-in the ADA4622-2? Answer The ADA4622-2 is available in both the photodiode wizard tool and the filter wizard tool available on www.analog.com.(http:…
  • Features of ADA4622-2

    Question What is the ADA4622-2? Answer The ADA4622-2 is the next generation of the AD822. It is a single supply, 30 V, 7.5 MHz, Low Bias Current, Single-Supply, RRO, Precision JFETOp Amp.
  • Noise performance of ADA4622-2

    Question How will the external circuitry affect the total noise performance? Answer The ADA4622-2 is designed for 12 nV/?Hz wideband input voltage noise and maintains low noise performance at low frequencies…
  • Phase reversal

    Question What about phase reversal? Answer The ADA4622-2 does not exhibit phase reversal for input voltages up to V+. For input voltages greater than V+, a 10 k? resistor in series with thenon-inverting…
  • Product grades of ADA4622-2

    Question What about product grades? Is there an A and B grade Answer Yes. Similar to other amplifiers the ADA4622-2 B-grade has the best performance offset voltage and offset voltage drift vs. temperature…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.