ADA4530-1: FAQ

  • Achieving femtoampere performance from the ADA4530-1R-EBZ evaluation board

    Question Why am I not achieving femtoampere performance from the ADA4530-1R-EBZ evaluation board? Answer One of the common reasons is contamination on the board. The effective insulation resistance of…
  • ADA4530-1: Where can I get EVAL-ADA4530-1 gerber files?

    Question Is it possible to get the gerber files of the evaluation board EVAL-ADA4530-1 ? There are not on your website product page. Answer See attached gerbers files for EVAL-ADA4530-1. These gerbers…
  • Advantages of ADA4530-1

    Question How is the ADA4530-1 better than its competitors? Answer The ADA4530-1 has input bias current that is guaranteed at ±20fA due to measurement limitations of a production environment even though…
  • Electrostatic interference

    Question How do I avoid electrostatic interference? Answer Very high impedance electrometer circuits are susceptible to interference through capacitive coupling. Interferences can be reduced with a shield…
  • Guard buffer connection in ADA4530-1

    Question Where is the guard buffer connected to internally? Answer The guard buffer is a unity-gain amplifier that creates a low-impedance replica of the amplifier input common- mode voltage. Internally…
  • Guarding techniques

    Question What are some common guarding techniques? Answer Guarding is important to completely surround the insulation of the high impedance node with another conductor that is driven to the guard voltage…
  • Key features and common applications of ADA4530-1

    Question What are the ADA4530-1 key features and what are the common applications it is used in? Answer The ADA4530-1 is an electrometer-grade operational amplifier with femtoampere (10-15) level input…
  • Package and evaluation board of ADA4530-1

    Question What package is the ADA4530-1 available in and is there an evaluation board available? Answer The ADA4530-1 amplifier is available in an 8-lead SOIC package. The amplifier is configured in transimpedance…
  • PCB dielectric/laminate material for ADA4530-1

    Question What PCB dielectric/laminate material should I be using with the ADA4530-1? Answer It is recommended to use the Rogers 4350B laminate with the ADA4530-1 in the highest performance applications…
  • Pin out of ADA4530-1

    Question Why does the ADA4530-1 have a unique pin out? Answer The ADA4530-1 provides an integrated guard buffer to isolate the input pins from leakage in the printed circuit board (PCB) and to minimize…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.