AD8421: FAQ

  • AD8421 Common Design Pitfalls to Avoid

    Question What are common pitfalls to avoid while designing with AD8421? Answer AD8421 is a high performance precision instrumentation amplifier, and as such, face certain situations for which it is unsuitable…
  • AD8421 Export Restrictions

    Question Are there export restrictions on the AD8421? Answer Instrumentation amplifiers are classified as an IC Amplifier per US export control standards, and are generally not subjected to export restrictions…
  • AD8421 Military Version

    Question So is there a military version of the AD8421? Answer Military applications often require exposure to hostile environments, such as higher temperature, higher pressure, and high reliability.…
  • AD8421 Robustness

    Question AD8421 is touted for its robustness. Can you give me some examples? Answer AD8421 is one of the most robust instrumentation amplifier on the market today. It features high ESD (Electrostatic…
  • AD8421 SOIC and MSOP Performance Differences

    Question Are there any performance differences between the AD8421 SOIC and MSOP package options? Answer There are some slight variations between specifications of the SOIC and MSOP. In general, the…
  • AD8421: Output impedance

    Question I am interested to know wich is the output resistance of the Instrumentation amplifier AD8421 becouse I need to compensate the effect of this one in the next stage of my design. Answer…
  • Buffer op amp for AD8421 REF pin

    Question I have a design using the AD8421 instrumentation amplifier with +20V and -5V supplies, the sense inputs have a common mode voltage between 0 and 15V and differential voltage of up to 140mV…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.