AD8336: FAQ

  • AD8336 Datasheet error in figure 77

    Question In the AD8336 datasheet, page 20, figure 77 (simplified block diagram showing depeaking capacitor), Rfb1 is connected between GND and PRAO. Is that correct? I would assume the connection…
  • AD8336: EVB header

    Question I have a question about AD8336's EVALZ Schematic. What's the function of VOUTL and VOUTD in the schematic of evaluation board? They seems like jumpers. (See attached Figure1). Answer The VOUTL…
  • AD8336_AN934 bandwidth change

    Question In Application Note AN-934 "60 dB Wide Dynamic Range, Low Frequency AGC Circuit" the circuit has output level flat over the audio frequency range of 20 Hz to 20 KHz. What changes are required…
  • AD8336_Power_Supply_issue

    Question One below customer is asking a question about AD8336. After his measurements, he still cannot get the gain value of 46db. But he mentioned, he cannot provide the -12V voltage when the supply…
  • AD8336_working at single 5V power supply

    Question Can AD8336 can be powered by single supply power, if it's OK, then how can I connect Vcom? Do I connect Vcom to mid supply? Answer The AD8336 can be used with a single supply. For a preliminary…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.