AD797: FAQ

  • AD797 ESD data HBM

    Question Do you have the ESD levels for the AD797? Answer Here are the ESD results for AD797: Passing level for HBM is 1.5kV and FICDM is 1.25kV
  • AD797: Maximum junction temperature Tj

    Question I can’t find the maximum junction temerature of AD797 in its datasheet. What is the value? Answer The max junction temperature is 150°C, same as other parts on the same process. By the way…
  • AD797: Offset Null configuration

    Question What range of potentiometer values do you recommend for the Offset Null Configuration? The data sheet (Page 14) shows a schematic with a 20kohm used; but there are no further notes? Answer…
  • Ad797: PSRR definition

    Question I would like to know if the power supply rejection ratio (PSRR) of the AD797 depends on the gain of the amplifier. Assuming a power supply with 100mVrms of 100Hz ripple and the circuit of…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.