AD210: FAQ

  • AD210 MTTF (MTBF) Data FAQ

    Q I am looking for the MTTF ( MTBF) data for the AD210. A please find attached Attachments: AD210qualification.pdf AD210_MTBF.PDF
  • AD210 output adjustment circuit

    Question we are currently using the „AD210JN“ as an input-amplifier in an industrial automation project. However, we have some issues with the “Vo” (Pin 1) and “Ocom” (Pin 2) output. We are trying…
  • AD210: low frequenc behavior of the AD210 - improve spec but not guaranteed after changed from TI TL082 to ADTL082

    Question Sometimes our measurement setup requires signal integration times of several seconds, so it is obvious that the low-frequency behavior of the AD210 is of importance to us. Now we are wondering…
  • AD210: Output current limit

    Question Do they have a current limit on the output of the isolation amplifier? If so what is the limit set at? Answer There is no current limit protection circuitry implemented on the AD210 output…
  • output short circuit

    Question Could you email me the amplifier output short circuit (not the power supply) specifications, Iout max?, type of load for this device? Etc. There is nothing on the data sheet. Answer The only…
  • ROHS compliancy for those parts?

    Question Does ADi plan a RoHS Compliant model? Answer ADI has no plans to convert the AD215 to a ROHS compliant model. It is an old design and not suitable for conversion to an EU-ROHS compliant material…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.