Is there a similar SDR based on AD9364 ?

Is there a similar SDR, like the ADALM-PLUTO but AD9364 based, not AD9363 as ADALM-PLUTO SDR? The AD9363 325 to 3800Mhz coverage is insufficient for some applications. The AD9364 coverage 70 to 6000 Mhz is much better in this sense.

Parents
  • 0
    •  Analog Employees 
    on Sep 2, 2017 1:48 AM

    1. With the software change I mentioned Pluto can operate the AD9363 at these bandwidths.  This is outside the datasheet spec though.

    2. The balun is speced 10MHz-6GHz I believe, so you are not limited there.  The schematics will give you the exact balun used.

    3. Currently no.  If you want to use the 9364 I would recommend the FMComms4.

Reply
  • 0
    •  Analog Employees 
    on Sep 2, 2017 1:48 AM

    1. With the software change I mentioned Pluto can operate the AD9363 at these bandwidths.  This is outside the datasheet spec though.

    2. The balun is speced 10MHz-6GHz I believe, so you are not limited there.  The schematics will give you the exact balun used.

    3. Currently no.  If you want to use the 9364 I would recommend the FMComms4.

Children
No Data