Is there a similar SDR, like the ADALM-PLUTO but AD9364 based, not AD9363 as ADALM-PLUTO SDR? The AD9363 325 to 3800Mhz coverage is insufficient for some applications. The AD9364 coverage 70 to 6000 Mhz is much better in this sense.
Travis,
Can you please clarify.
1. Pluto board image (attached) clearly shows AD9363 chip used.
Is this correct that AD9363 can be used outside of specified 325-3800 Mhz, 20Mhz bandwidth
http://www.analog.com/media/en/technical-documentation/data-sheets/AD9363.pdf
I.e. is is correct that AD9363 can do 56Mhz bandwidth?
2. Pluto board has input transformer (clearly seen on image). It will unlikely to work well for 70-6000
if it was designed for 325-3800.
3. Can a Pluto board with AD9364 be sold (or intended to be manufactured in the future).
Vladislav