Post Go back to editing

OFDM modülation live data stream with Adalm-pluto

Category: Software
Product Number: ADALM-PLUTO
Software Version: v0.37

We are trying to create OFDM-QPSK symbols modulation and demodulation with two Adalm pluto sdr 9363 Revision C. We are using OFDM parameters in 802.11g standard by using Analog Device SDR book. However, we are experiencing synchronization problem even in very small bit packets. CFO is 500-600 kHz and BER is at least 50%, there is no channel coding. Frame cannot be captured properly in receiver. We are doing all these operations in matlab. What do you think could be the problem?