Hi,
I try to setup a OOK (On-Off Keying) modulation with my PlutoSDR but I face some issues.
I want to generate a signal with a carrier of 868 MHz and a datarate of 2Mbaud.
I finally succed to generate a signal but i'm a bit disturbing by the rise/fall time between bit.
I find that the rise/fall time are very long.
I expected something much shorter.
I use the following C code with libiio and libad9361 to drive the device.
Right now this code only generate a sequence of 100 bit "01010101..." and convert it to IQ sample data to send it every ms.
There is a better way to generate the signal to have a much shorter rise/fall time ?
srimoyi - Moved from Design Support AD9361/AD9363/AD9364 to Virtual Classroom for ADI University Program. Post date updated from Friday, March 21, 2025 11:26 AM UTC to Monday, March 24, 2025 8:58 AM UTC to reflect the move.
srimoyi - Moved from Design Support AD9361/AD9363/AD9364 to Virtual Classroom for ADI University Program. Post date updated from Monday, March 24, 2025 8:58 AM UTC to Monday, March 24, 2025 8:58 AM UTC to reflect the move.
Moving to appropriate forum for questions on Pluto.