I have been running the Range_Doppler_Plot.py code in my backyard to collect data files, and also using the Range_Doppler_Processing.py code to view the files for additional analysis. I saved a data file that is ~330 MB that I would like to share with you so you can look at the clutter cancellation of the code. The data file was created with me walking 20-meters away from the Phaser system, and then walking back to the Phaser to stop the data collection. The file is saved in Google Drive, so I will need an e-mail address for someone at Analog Devices so they can download the file to view it using Range_Doppler_Processing.py.
I am walking 20-meters, where I encounter two Blue Spruce trees in the backyard, so that limits the distance that I can traverse in that direction. The Clutter is very bad, even though the data was collected using 2 Pulse Clutter Cancellation, and the image appears as follows:
Can I do anything else with the Range_Doppler_Plot.py code to reduce the clutter, or is the best that can be obtained?