Post Go back to editing

Transmitting and Receiving Visual Data Using OFDM with a Single SDR

Category: Software

Hello, I am new to developing projects on PlutoSDR. The project I want to create involves converting an image into bits, encoding it, passing it through OFDM modulation, and transmitting and receiving it via SDR. For this, I first encoded a 320x240x8-bit image using a 1/2 convolutional encoder. Then, I applied QPSK modulation, resulting in a total of 614,400 symbols. I chose an SCS of 30 kHz and an FFT size of 1024, and placed these symbols into 4 5G radio frames as follows: each slot consists of 14 symbols, with 80 slots in total. The first 13 symbols of each slot contain 45 resource blocks, and the last symbol contains 55 resource blocks. Each resource block consists of 12 resource elements. ((13*45+55)*12)*80 = 614,400. Before applying OFDM modulation, I added a Barker code that fits into 2 resource blocks to detect the frame start at the receiver. The spectrum of the signal I generated for transmission seems correct, but the received signal appears to be meaningless. I suspect this is because I did not set the SDR TX and RX parameters correctly. I wrote the code in Python. Based on the system I created, how should I set the SDR's sample rate, TX and RX bandwidth, and RX buffer size?