Post Go back to editing

Different Tx power in consecutive repeatTransmit executions, with the same exact settings (Adalm Pluto)

Category: Hardware
Product Number: adalm pluto

I am seeing that, each time I do a repeatTransmit (under the same configuration), I observe different output levels, apparently in a random way. Both output levels are influenced by the Attenuation selected. For example, the plots below are two consecutive executions of the same Matlab code:

Example with "low" output power:

Example with "high" output power

What is the origin of this? Is this indicating a HW problem? 

I would be very grateful for any guidance understanding what is happening here.

Best regards,

Thread Notes

Parents Reply Children
  • Hi Travis, thank you for your suggestion & prompt response. Selecting an in-band frequency provides the same inconsistent output power between runs. I am using the following code:

    txGain = -50;

    Fs = 3e6;
    fc = 1.290e9;
    tx = sdrtx(deviceNameSDR);
    tx.RadioID = 'ip:192.168.2.1';
    tx.CenterFrequency = 1.290e9;
    tx.BasebandSampleRate = Fs;
    tx.Gain = txGain;
    sw = dsp.SineWave;
    sw.Amplitude = 10;
    sw.Frequency = Fs/4;
    sw.ComplexOutput = true;
    sw.SampleRate = Fs;
    sw.SamplesPerFrame = 20000;
    txWaveform = sw();
    transmitRepeat(tx,txWaveform);
    release(tx);
    Any further idea? I also tried DDS with the same result.
    Thanks again for your help.
  • After further testing, I've managed to solve this issue. This seems originated by an incompatibility between the firmware in the Pluto (v0.38) and the firmware expected by Matlab (v0.34). If v0.34 is installed in the Pluto, the issue is resolved.

    Thanks again Travis for your assistance.