Good afternoon,
I have run into an issue when trying to set the PLUTO SDR (firmware version 0.38) to a 2-channel RX mode in a Python script. The mode is already set to 2r2t on the device itself (verified by ssh'ing into the PLUTO and using fw_printenv mode), but when I put together a simple script to capture a few samples on both RX channels (e.g. following the steps as described on this page), the following line in the script:
sdr.rx_enabled_channels = [0, 1]
gives me the error message:
Exception: RX mapping exceeds available channels
I am not sure why this happens. I am probably missing something, because we have been using this device in 2-channel RX mode just fine using other scripts. I unfortunately can't copy the initialisation steps from there as we use a different way to initialise the PLUTO there, with a JSON file.
For completeness' sake, the full script is listed below.
import numpy as np
import adi
import datetime
sample_rate = 521000 # Hz, 25 Ms/48 decimation rounded up
center_freq = 1451e6 # Hz
num_samps = 521000 # number of samples returned per call to rx()
sdr = adi.Pluto('ip:192.168.2.1')
sdr.rx_enabled_channels = [0, 1]
sdr.gain_control_mode_chan0 = 'manual'
sdr.gain_control_mode_chan1 = 'manual'
sdr.rx_hardwaregain_chan0 = 70.0 # dB
sdr.rx_hardwaregain_chan1 = 70.0 # dB
sdr.rx_lo = int(center_freq)
sdr.sample_rate = int(sample_rate)
sdr.rx_rf_bandwidth = int(sample_rate)
sdr.rx_buffer_size = num_samps
count = 0
while (count < 10):
samples = sdr.rx()
count = count + 1
print(datetime.datetime.now())
Any thoughts would be much appreciated!
Found the mistake! I needed to use adi.ad9361('ip:192.168.2.1') instead of adi.Pluto('ip:192.168.2.1') in order to enable 2-channel readout. The script works as expected now, returning 2 data arrays into the samples variable.