Post Go back to editing

Bug on FMComms block when running Pluto on Raspberry's GNURadio

Category: Software

Hi,

I am using the "enhanced Pluto" AD9361 2rx,2tx on the Raspberry's GNURadio 8. (I followed Jon's Kraft video here: https://www.youtube.com/watch?v=ph0Kv4SgSuI)

I have found FMCOMMS2/3/4 Sink (and source) does not work when having the following setup:

Using only one TX,RX, when you 

"Enable TX2" -> FMCOMMs2/3/4 Sink

"Enable RX2"->FMCOMMs2/3/4 Source

the gnuradio flowgraph cannot execute. 

Enabling TX1,RX1 will work fine. The issue are the Channel 2. A similar bug is reported in:  Pluto with 2 RX channels using GNURadio 

The workaround only works for GNURADIO 3.10 and above. (Running in the Raspberry is only 3.8). 

Is there any way to update the fmcomms blocks to the latest on 3.8 ?