Hi Jon!
This time I need your help in some confirmation, I want to replace PLUTO with USRP either I will generate FMCW signal using USRP or from Pluto but will receive back signal from phaser to USRP. For Only receiving part I think I need to change the connection that is triggering PLUTO receiver. I will connect that pin to one of digital I/P of USRP to trigger its FIFO receive the actual number of data points and then wait for next trigger and this will continue. For that I think the trigger pin to PLUTO receiver will be that which one is coming to I10P. Correct me if I am wrong, please.
Also discuss the case where I will be transmitting and receiving both using USRP then what should be the configuration for those 14 pins header of phaser. Please explain their usage.
majorly I want to know what essentials for chirp synchronization are.
Thankyou
I'm not sure how it would work with the USRP. I'm sure there is a way to do it, but I don't know how. But you can find an explanation of the signals for Pluto and Phaser in these 2 videos:
https://www.youtube.com/live/PVlWK-39cCw?si=sYkbPo_qqxL8FQpR&t=26955
Thank you, these links were helpful as they provide more in-depth knowledge about TDD engine. But I was asking you to just tell me that which pin is triggering PLUTO Rx buffer, and which PIN is triggering CN0566 phaser Tx to start frequency ramp for FMCW. Then I will use these triggers to sync my USRP code.
Moreover, basically I want to understand in detail working mechanism of that 14 Pin header on PLUTO & PHASER, that which pin is responsible for which work. Please if you can help me.
Thankyou
Yes, all those details are in the referenced videos above. I would rather you see the answers in context of the full solution, as it may help you with follow up questions.