I have followed this lab: 2_axis_tilt_sensor
I am using the ADALM1000 instead of 2000 and I have also used a small voltage inverter from Polulu to get -5v as well as +5 into the comparator side of the circuit as the ADALM1000 cannot produce a negative voltage. I am using 3.3v from ADALM1000 to power the sensor itself.
I am having the problem that the LEDs that go from the non-inverting OUT of both AD8561s (pins #7) are on at start-up. In the picture, they are the green LEDs. Is this the right behaviour? Should all the LEDs be off at start-up?
Any help or feedback would be appreciated. This lab is also available in the Studentzone vol. 57 No.3-September 2023
Here is a picture of my breadboard. Note: I am using LEDs with built-in resistors: