Hello,
I am trying to run the Phaser CN0566 code for FMCW radar by Jon.Kraft on a ADLAM-Pluto that I've hacked by using the steps given by Jon on his youtube channel, But as I don't need two TX/RX channels so I've just increased the pluto's bandwidth.
I've written a spectrum analyzer like code for the pluto bas per my requirements and removed the parts of code that are required by phaser.
When I run the code the GUI starts but as I press Start the pluto throws a connection time out error at the sdr.rx() line.
I have checked and I my software versions all satisfy the the requirements put forward by Jon Kraft in his youtube video.
I use a bin file to load the data so that there should not be any load on the PC the parameters I use in the bin file are
fs = 5e6 #sampling frequency
bandwidth = 750e3
on_time = 0.9e-3 # sec
off_time = 0.1e-3
onsamp = 4096
off_samp = 1024
Below is the code for the GUI
from PyQt5.QtWidgets import QApplication, QMainWindow, QVBoxLayout, QHBoxLayout, QWidget, QPushButton, QLabel from PyQt5.QtCore import Qt, QTimer import numpy as np import pyqtgraph as pg import adi import sys class RealTimeFFTWindow(QMainWindow): def __init__(self): super().__init__() # file_path = 'calc.iq' file_path = 'pylfm.iq' self.tx_data = np.fromfile(file_path, dtype=np.complex64) self.tx_data *= 2**14 # Initialize the PlutoSDR self.center_frequency = int(435e6) self.buffer_size = int(len(self.tx_data)) self.bandwidth = int(750e3) self.sample_rate = int(5e6) self.period = 200e-6 self.buffers = np.array([], dtype = np.complex64) try: # self.sdr = adi.Pluto(uri="usb:1.8.5") self.sdr = adi.Pluto(uri="ip:192.168.2.1") # Adjust IP address as necessary self.sdr.rx_lo = self.center_frequency # self.sdr.filter = 'AD936x_LP_666kHz_2MSPS.ftr' self.sdr.sample_rate = self.sample_rate self.sdr.rx_rf_bandwidth = self.bandwidth self.sdr.rx_hardwaregain_chan0 = 0.0 self.sdr.rx_buffer_size = self.buffer_size except Exception as e: print(f"Error initializing PlutoSDR: {e}") sys.exit(1) # Array to store received samples self.received_samples = np.array([], dtype=np.complex64) self.sdr.tx_rf_bandwidth = self.bandwidth self.sdr.tx_lo = self.center_frequency self.sdr._tx_buffer_size = self.buffer_size self.sdr.gain_control_mode_chan0 = "manual" self.sdr.tx_hardwaregain_chan0 = 0.0 # the range is -90 to 0 dB self.sdr.tx_cyclic_buffer = True # Enable cyclic buffers # Configure TDD controller sdr_pins = adi.one_bit_adc_dac(uri="ip:192.168.2.1") sdr_pins.gpio_tdd_ext_sync = False # If set to True, this enables external capture triggering using the L24N GPIO on the Pluto. When set to false, an internal trigger pulse will be generated every second tdd = adi.tddn(uri="ip:192.168.2.1") tdd.enable = False # disable TDD to configure the registers tdd.sync_external = True tdd.startup_delay_ms = 0 tdd.frame_length_ms = self.period/1e3 + 0.2 # each chirp is spaced this far apart num_chirps = 1 tdd.burst_count = num_chirps # number of chirps in one continuous receive buffer tdd.channel[0].enable = True tdd.channel[0].polarity = False tdd.channel[0].on_ms = 0.01 tdd.channel[0].off_ms = 0.1 tdd.channel[1].enable = True tdd.channel[1].polarity = False tdd.channel[1].on_ms = 0.01 tdd.channel[1].off_ms = 0.1 tdd.channel[2].enable = False tdd.enable = True # # Pluto receive buffer size needs to be greater than total time for all chirps # total_time = tdd.frame_length_ms * num_chirps # time in ms # print("Total Time for all Chirps: ", total_time, "ms") # buffer_time = 0 # power=12 # while total_time > buffer_time: # power=power+1 # buffer_size = int(2**power) # buffer_time = buffer_size/self.sdr.sample_rate*1000 # buffer time in ms # if power==23: # break # max pluto buffer size is 2**23, but for tdd burst mode, set to 2**22 # print("buffer_size:", buffer_size) # self.sdr.rx_buffer_size = buffer_size # print("buffer_time:", buffer_time, " ms") # Set up the GUI self.setWindowTitle("SAR GUI") self.setGeometry(400, 100, 1200, 800) central_widget = pg.GraphicsLayoutWidget() self.setCentralWidget(central_widget) layout = QHBoxLayout(central_widget) plot_panel = QWidget() plot_layout = QVBoxLayout(plot_panel) # Add side control panel side_panel = QWidget() side_layout = QVBoxLayout(side_panel) side_panel.setFixedWidth(220) layout.addWidget(plot_panel) layout.addWidget(side_panel) # Add label widget for displaying coordinates and data self.label = QLabel() self.label.setStyleSheet("color: yellow;") self.label.setAlignment(Qt.AlignRight) # Add PlotWidgets for FFT and Time Domain self.fft_plot = pg.PlotWidget(title="Beat Signal FFT") self.timedomain_plot = pg.PlotWidget(title="Time Domain") plot_layout.addWidget(self.timedomain_plot) plot_layout.addWidget(self.label) plot_layout.addWidget(self.fft_plot) # FFT Curve self.curve_fft_below = self.fft_plot.plot(pen=pg.mkPen(color="limegreen", width=1.5), fillLevel=-110, fillBrush=(50, 50, 200, 100)) self.curve_fft_above = self.fft_plot.plot(pen=pg.mkPen(color="limegreen", width=1.5), fillLevel=30, fillBrush=(1, 1, 1, 100)) self.curve_fft_max_hold = self.fft_plot.plot(pen=pg.mkPen(color="red", width=1.5), fillLevel=30) # Time Domain Plot Controls self.vLine_time = pg.InfiniteLine(angle=90, movable=False) self.hLine_time = pg.InfiniteLine(angle=0, movable=False) self.timedomain_plot.addItem(self.vLine_time, ignoreBounds=True) self.timedomain_plot.addItem(self.hLine_time, ignoreBounds=True) # Set background color to dark gray self.fft_plot.setBackground('#222222') self.timedomain_plot.setBackground('#222222') # Add controls to the side panel self.start_button = QPushButton("Start") self.start_button.clicked.connect(self.start_update) self.start_button.clicked.connect(self.transmit) self.start_button.setStyleSheet("background-color: green;") side_layout.addWidget(self.start_button) self.max_hold_button = QPushButton("Max Hold") self.max_hold_button.clicked.connect(self.toggle_max_hold) self.max_hold_button.setStyleSheet("background-color: white;") side_layout.addWidget(self.max_hold_button) side_layout.addStretch() # Crosshair lines self.vLine = pg.InfiniteLine(angle=90, movable=False) self.hLine = pg.InfiniteLine(angle=0, movable=False) self.fft_plot.addItem(self.vLine, ignoreBounds=True) self.fft_plot.addItem(self.hLine, ignoreBounds=True) # Mouse movement event handling self.proxy_fft = pg.SignalProxy(self.fft_plot.scene().sigMouseMoved, rateLimit=60, slot=self.mouseMovedFFT) self.proxy_time = pg.SignalProxy(self.timedomain_plot.scene().sigMouseMoved, rateLimit=60, slot=self.mouseMovedTime) # Variables for real-time update self.update_interval = 10 # milliseconds self.timer = QTimer() self.timer.timeout.connect(self.update_plot) self.is_running = False self.max_hold_enabled = False self.max_hold_data = None # Add x and y labels to FFT plot self.fft_plot.setLabel('left', text='Power (dB)') self.timedomain_plot.setLabel('bottom', text='Time') self.timedomain_plot.setLabel('left', text='Amplitude') def mouseMovedFFT(self, evt): pos = evt[0] # Using signal proxy turns original arguments into a tuple if self.fft_plot.sceneBoundingRect().contains(pos): mousePoint = self.fft_plot.plotItem.vb.mapSceneToView(pos) x = mousePoint.x() y = mousePoint.y() # Convert x from plot coordinate to frequency in MHz freq_mhz = x self.vLine.setPos(x) self.hLine.setPos(y) self.label.setText(f'Frequency: {freq_mhz:.2f} MHz, Power: {y:.2f} dB') def mouseMovedTime(self, evt): pos = evt[0] if self.timedomain_plot.sceneBoundingRect().contains(pos): mousePoint = self.timedomain_plot.plotItem.vb.mapSceneToView(pos) x = mousePoint.x() y = mousePoint.y() # Convert x from plot coordinate to time in seconds time_sec = x self.vLine_time.setPos(x) self.hLine_time.setPos(y) self.label.setText(f'Time: {time_sec:.2f} s, Amplitude: {y:.2f}') def start_update(self): if not self.is_running: self.timer.start(self.update_interval) self.is_running = True self.start_button.setText("Stop") self.start_button.setStyleSheet("background-color: red;") else: self.timer.stop() self.is_running = False self.start_button.setText("Start") self.start_button.setStyleSheet("background-color: green;") # Stop the SDR and save data self.stop_sdr() self.save_received_samples() def toggle_max_hold(self): self.max_hold_enabled = not self.max_hold_enabled if self.max_hold_enabled: self.max_hold_button.setText("Max Hold (Enabled)") self.max_hold_button.setStyleSheet("background-color: gray;") self.max_hold_data = None # Reset max hold data else: self.max_hold_button.setText("Max Hold") self.max_hold_button.setStyleSheet("background-color: white;") def transmit(self): self.sdr.tx(self.tx_data) def update_plot(self): rx_samples = self.sdr.rx() # Handle mismatch in lengths if len(rx_samples) != len(self.tx_data): print("Mismatch in transmitted and received data lengths.") if len(rx_samples) > len(self.tx_data): rx_samples = rx_samples[:len(self.tx_data)] print("Mismatch Fixed.") else: rx_samples = np.pad(rx_samples, (0, len(self.tx_data) - len(rx_samples)), 'constant') print("Mismatch Fixed.") # Store the received samples in the array self.received_samples = np.concatenate((self.received_samples, rx_samples)) # Multiply transmitted and received pulses beat_signal = self.tx_data * np.conj(rx_samples) window = np.hanning(len(beat_signal)) beat_signal_windowed = window * beat_signal # Time Domain iq_time = np.linspace(0, len(rx_samples) / self.sdr.sample_rate, len(rx_samples)) self.timedomain_plot.plot(iq_time, rx_samples.real, pen='limegreen', clear=True) # FFT update beat_signal_fft = np.fft.fftshift(np.fft.fft(beat_signal_windowed)) # Calculate the frequency axis freq_axis = np.fft.fftshift(np.fft.fftfreq(len(beat_signal_fft), d=1/self.sdr.sample_rate)) freq_axis_mhz = freq_axis / 1e6 # Convert to MHz # Update plot with axis limits and tick formatting self.fft_plot.setXRange(freq_axis_mhz[0], freq_axis_mhz[-1], padding=0) tick_step = 5 # Define the step for ticks in MHz tick_positions = np.arange(freq_axis_mhz[0], freq_axis_mhz[-1] + tick_step, tick_step) tick_labels = [f"{v:.2f} MHz" for v in tick_positions] self.fft_plot.getAxis('bottom').setTicks([list(zip(tick_positions, tick_labels))]) beat_signal_fft_db = 20 * np.log10(np.abs(beat_signal_fft) + 1e-6) # Added small offset to avoid log(0) baseline = np.mean(beat_signal_fft_db[:100]) baseline_adjustment = -90 - baseline beat_signal_fft_db_corrected = beat_signal_fft_db + baseline_adjustment threshold = -90 # Adjust threshold level as needed beat_signal_fft_db_corrected[beat_signal_fft_db_corrected < threshold] = threshold if self.max_hold_enabled: if self.max_hold_data is None: self.max_hold_data = beat_signal_fft_db_corrected else: self.max_hold_data = np.maximum(self.max_hold_data, beat_signal_fft_db_corrected) self.curve_fft_max_hold.setData(freq_axis_mhz, self.max_hold_data, connect='all', antialias=True) else: self.curve_fft_max_hold.setData([], []) self.curve_fft_above.setData(freq_axis_mhz, beat_signal_fft_db_corrected, connect='all', antialias=True) def stop_sdr(self): # Stop the transmission and reception self.sdr.tx_destroy_buffer() self.sdr.rx_destroy_buffer() print("SDR transmission and reception stopped.") def save_received_samples(self): # Save the received samples to a binary file output_file = "received_samples.bin" self.received_samples = self.received_samples.astype(np.complex64) self.received_samples.tofile(output_file) print(f"Received samples saved to {output_file}") if __name__ == "__main__": app = QApplication(sys.argv) window = RealTimeFFTWindow() window.show() sys.exit(app.exec_())
Traceback (most recent call last): File "/home/oem/ADVR9361/SAR.py", line 443, in update_plot rx_samples = self.sdr.rx() File "/home/oem/.local/lib/python3.8/site-packages/adi/rx_tx.py", line 248, in rx data = self.__rx_complex() File "/home/oem/.local/lib/python3.8/site-packages/adi/rx_tx.py", line 213, in __rx_complex x = self._rx_buffered_data() File "/home/oem/.local/lib/python3.8/site-packages/adi/compat.py", line 149, in _rx_buffered_data self._rxbuf.refill() File "/home/oem/.local/lib/python3.8/site-packages/iio.py", line 1003, in refill _buffer_refill(self._buffer) File "/home/oem/.local/lib/python3.8/site-packages/iio.py", line 62, in _check_negative raise OSError(-result, _strerror(-result)) TimeoutError: [Errno 110] Connection timed out
Timeout means that it takes too long for the device to respond. What are the buffersizes/samplerates you expect to receive ? If these are fine, ithen it's probably some of the synchronization pieces that do not trigger properly.
Hello ASuciu,
Thank you for your quick reply.
What are the buffersizes/samplerates you expect to receive ?
Without the TDD controller part the spectrum analyser runs perfectly, but since I added the TDD controller part the code gives this error.
If these are fine, ithen it's probably some of the synchronization pieces that do not trigger properly.
Yeah that's what I too was thinking so I tried to search if there are any sample codes that I can try to run first then I'll try to make changes in my code but I found none,
And in the video Jon had said that for most cases the values of the attributes in the TDD part will be the same.
Will you be able to help me debug the code?
Regards,
Hello ASuciu,
Thank you for your quick reply.
What are the buffersizes/samplerates you expect to receive ?
Without the TDD controller part the spectrum analyser runs perfectly, but since I added the TDD controller part the code gives this error.
If these are fine, ithen it's probably some of the synchronization pieces that do not trigger properly.
Yeah that's what I too was thinking so I tried to search if there are any sample codes that I can try to run first then I'll try to make changes in my code but I found none,
And in the video Jon had said that for most cases the values of the attributes in the TDD part will be the same.
Will you be able to help me debug the code?
Regards,
Yes, if you're not using the GPIO on the Phaser to trigger the start of TDD, then you'll need to send it a software trigger command (tdd.sync_soft). Try something like this:
# %% Setup TDD Timing
# Enable phaser logic in pluto
gpio = adi.one_bit_adc_dac(sdr_ip)
time.sleep(0.1)
gpio.gpio_phaser_enable = True # when true, each channel[1] start outputs a pulse to Pluto L10P pin (TXDATA_1V8 on Phaser schematic)
time.sleep(0.1)
# Configure TDD properties
tdd = adi.tddn(sdr_ip)
tdd.enable = False # make sure the TDD is disabled before changing properties
tdd.frame_length_ms = 520 # each burst (L10P toggle) is spaced this apart
tdd.startup_delay_ms = 0 # startup delay
tdd.burst_count = 1 # number of bursts in a row
tdd.channel[0].enable = True
tdd.channel[0].polarity = False
tdd.channel[0].on_ms = 0.0
tdd.channel[0].off_ms = 0.2
tdd.channel[1].enable = True
tdd.channel[1].polarity = False
tdd.channel[1].on_ms = 0.0
tdd.channel[1].off_ms = 0.2
tdd.channel[2].enable = False
tdd.channel[2].polarity = False
tdd.channel[2].on_ms = 0
tdd.channel[2].off_raw = 10
tdd.sync_external = True # enable external sync trigger
tdd.sync_internal = False # enable the internal sync trigger
tdd.enable = True # enable TDD engine
# transmit data from Pluto
my_sdr._ctx.set_timeout(30000)
time.sleep(0.5)
my_sdr._rx_init_channels()
time.sleep(0.5)
tdd.enable = False
tdd.channel[2].enable = True
my_sdr.tx([iq_chirp, iq_chirp])
tdd.enable = True
# Receive data
tdd.sync_soft = 1
data = my_sdr.rx()
Thank you, Jon the code runs fine now but I still am facing problem I think that I has some thing to do with the synchronization of the TX and the RX channels or the fact that as my distance between the Transmitter-Target-Reciver is very less so the wave is instantaneously received at the receiver, even though I am using a RF cable of 5m length I can see the beat frequency moving all over the frequency spectrum. My gui code also stores each received buffer in a single array which is then stored as a bin file when we stop the transmission, and when I plot that bin file I see that the buffers are either overlapped or some samples are being dropped and not received but that does not happen in your case on the phaser, could you please help me to understand what parameters are causing this error.
Below is the figure showing the overlap of the buffers
Regards,
Deadshot
I'm working with the software developers now on a better way to synchronize this, and with greater accuracy. I think we're close to a solution (new firmware for Pluto). But in the meantime, you can try this more cumbersome approach:
for i in range(1): tdd.enable = False my_sdr.tx_destroy_buffer() my_sdr.tx([iq, iq]) tdd.channel[2].enable = True tdd.enable = True tdd.sync_soft =True data = my_sdr.rx()