Hello to everyone,
I'm experiencing an issue with my Adalm-Pluto SDR kit, which is equipped with a Zynq Z-7000 SoC. I'm using Vivado to program the SoC and a Xilinx Platform Cable USB II for connecting the Pluto to Vivado. Previously, Vivado was able to detect the Pluto as a target device, but now I'm encountering a problem where Vivado no longer recognizes it.
The error I receive is this:
"[Labtools 27-2269] No devices detected on target localhost:3121/xilinx_tcf/Xilinx/00001dcff8b301.
Check cable connectivity and that the target board is powered up then
use the disconnect_hw_server and connect_hw_server to re-register this hardware target."
Here are the things I've done to solve the issue:
- Checked the cable connections to ensure they are secure.
- Uninstalled and reinstalled the drivers for the Xilinx Platform Cable USB II.
- Restarted Vivado and the hardware server multiple times.
As for the cable connections:
- I have connected TDI, TDO, TCK, TMS to their respective ports on the Pluto.
- Both the platform's ground and Pluto's ground are connected to a common ground.
- The platform's VREF is connected to 3.6 Volts.
- The Pluto is connected to the computer via USB.
- The JTAG_Boot pin is connected to the same common ground as both devices.
For better understanding of the cable connections you can view the following pictures. I would really appreciate any assistance or suggestions on how to resolve this issue. Thank you for your attention and support.