hi i m a novice, need help in translating the GNURADIO bandlimited threshold detector -wiki.gnuradio.org/index.php
the purpose is the sweep the spectrum fro 70 mhz to 6ghz and record the active frequencies with their power
can anyone help me out - i have Analog Devices PlutoSDR Rev.B (Z7010-AD9364) connected to my windows 10 pc
travisfcollins - Moved from RF and Microwave to Virtual Classroom for ADI University Program. Post date updated from Sunday, January 28, 2024 8:11 PM UTC to Monday, January 29, 2024 2:24 PM UTC to reflect the move.
To change the LO frequency in GR programmatically, there are two ways that come to mind. You could restart the flowgraph each time with a new LO setting for pluto. This is just a small change to the generated flowgraph in Python and introduce a loop. Or you could use the Attribute Sink block to do an attribute update for the LO frequency property of the device: https://wiki.analog.com/resources/tools-software/linux-drivers/iio-transceiver/ad9361#local_oscillator_control_lo
-Travis
hi i have tried but failed, see attached flowgraph drive.google.com/.../1EV5vlCO6T93sB7cd1FBxEsR5SQJ05sOP, can you help to correct what am i missing to show the full spectrum instead of the moving spectrum.
also how to connect it as input to the detector in the bandlimited threshold detector example
i tried in python too but something is wrong there also. i cant get the whole spectrum to be displayed at one go - python code also in the same folder shared above myscanner.py
I cannot access that link. Can you post the raw text here through the "insert" option or use pastebin/github-gist?
-Travis
thanks travis - please find files at https://file.io/gWWwOSUBR7WL
What is the problem you are observing?
-Travis
i am only able to get a portion of the spectrum value charted whereas i want to show the full spectrum range that the sdr has. Also i could not figure out how to merge the bandwidth threshold logger flowgrah to be adapted to a realword sdr
i am only able to get a portion of the spectrum value charted whereas i want to show the full spectrum range that the sdr has.
What is limiting this?
-Travis
Dear Travis,
my knownledge is limiting me create a flowgraph suitable for the purpose
please have a look at the flowgraph and advise what needs to be corrected, currently the fft is on autoscroll for the current bandwidth in centre.
Appreciate your support
code as below for grc
options: parameters: author: navneet catch_exceptions: 'True' category: '[GRC Hier Blocks]' cmake_opt: '' comment: '' copyright: '' description: '' gen_cmake: 'On' gen_linking: dynamic generate_options: qt_gui hier_block_src_path: '.:' id: sweeperbyalienai23 max_nouts: '0' output_language: python placement: (0,0) qt_qss_theme: '' realtime_scheduling: '' run: 'True' run_command: '{python} -u {filename}' run_options: prompt sizing_mode: fixed thread_safe_setters: '' title: Frequency Sweeper window_size: (1000,1000) states: bus_sink: false bus_source: false bus_structure: null coordinate: [8, 8] rotation: 0 state: enabled blocks: - name: bandwidthrx id: variable parameters: comment: '' value: '5200000' states: bus_sink: false bus_source: false bus_structure: null coordinate: [1168, 8.0] rotation: 0 state: true - name: freq id: variable parameters: comment: '' value: python_mod.sweeper(fun_prob) states: bus_sink: false bus_source: false bus_structure: null coordinate: [552, 16.0] rotation: 0 state: enabled - name: freqmim id: variable_qtgui_range parameters: comment: '' gui_hint: '' label: 'Frequency Min ' min_len: '200' orient: QtCore.Qt.Horizontal rangeType: float start: '0' step: '1000000' stop: '6000000000' value: '70000000' widget: counter_slider states: bus_sink: false bus_source: false bus_structure: null coordinate: [1336, 4.0] rotation: 0 state: true - name: frequency id: variable_qtgui_label parameters: comment: '' formatter: None gui_hint: '' label: 'Frequency ' type: real value: freq states: bus_sink: false bus_source: false bus_structure: null coordinate: [680, 4.0] rotation: 0 state: true - name: fun_prob id: variable_function_probe parameters: block_id: probSign comment: '' function_args: '' function_name: level poll_rate: '10' value: '0' states: bus_sink: false bus_source: false bus_structure: null coordinate: [8, 428.0] rotation: 0 state: true - name: samp_rate id: variable parameters: comment: '' value: '56000000' states: bus_sink: false bus_source: false bus_structure: null coordinate: [8, 120.0] rotation: 0 state: enabled - name: variable_qtgui_label_0 id: variable_qtgui_label parameters: comment: '' formatter: None gui_hint: '' label: amp type: real value: '0' states: bus_sink: false bus_source: false bus_structure: null coordinate: [8, 188.0] rotation: 0 state: true - name: analog_noise_source_x_0 id: analog_noise_source_x parameters: affinity: '' alias: '' amp: '1' comment: '' maxoutbuf: '0' minoutbuf: '0' noise_type: analog.GR_GAUSSIAN seed: '0' type: float states: bus_sink: false bus_source: false bus_structure: null coordinate: [280, 164.0] rotation: 0 state: disabled - name: analog_sig_source_x_0 id: analog_sig_source_x parameters: affinity: '' alias: '' amp: '1' comment: '' freq: '0' maxoutbuf: '0' minoutbuf: '0' offset: '0' phase: '0' samp_rate: samp_rate type: complex waveform: analog.GR_CONST_WAVE states: bus_sink: false bus_source: false bus_structure: null coordinate: [8, 284.0] rotation: 0 state: disabled - name: analog_sig_source_x_1 id: analog_sig_source_x parameters: affinity: '' alias: '' amp: '1' comment: '' freq: freq maxoutbuf: '0' minoutbuf: '0' offset: '0' phase: '0' samp_rate: samp_rate type: float waveform: analog.GR_COS_WAVE states: bus_sink: false bus_source: false bus_structure: null coordinate: [280, 4.0] rotation: 0 state: disabled - name: blocks_add_xx_0 id: blocks_add_xx parameters: affinity: '' alias: '' comment: '' maxoutbuf: '0' minoutbuf: '0' num_inputs: '2' type: float vlen: '1' states: bus_sink: false bus_source: false bus_structure: null coordinate: [600, 136.0] rotation: 0 state: disabled - name: blocks_throttle_0 id: blocks_throttle parameters: affinity: '' alias: '' comment: '' ignoretag: 'True' maxoutbuf: '0' minoutbuf: '0' samples_per_second: samp_rate type: complex vlen: '1' states: bus_sink: false bus_source: false bus_structure: null coordinate: [280, 328.0] rotation: 0 state: disabled - name: blocks_throttle_0_0 id: blocks_throttle parameters: affinity: '' alias: '' comment: '' ignoretag: 'True' maxoutbuf: '0' minoutbuf: '0' samples_per_second: samp_rate*4 type: complex vlen: '1' states: bus_sink: false bus_source: false bus_structure: null coordinate: [1008, 512.0] rotation: 0 state: disabled - name: fft_vxx_0 id: fft_vxx parameters: affinity: '' alias: '' comment: '' fft_size: '1024' forward: 'True' maxoutbuf: '0' minoutbuf: '0' nthreads: '1' shift: 'True' type: float window: window.blackmanharris(1024) states: bus_sink: false bus_source: false bus_structure: null coordinate: [1256, 420.0] rotation: 0 state: disabled - name: iio_pluto_source_0 id: iio_pluto_source parameters: affinity: '' alias: '' bandwidth: bandwidthrx bbdc: 'True' buffer_size: '32768' comment: '' filter: '' filter_source: '''Auto''' fpass: '0' frequency: freq fstop: '0' gain1: '''manual''' len_tag_key: packet_len manual_gain1: '64' maxoutbuf: '0' minoutbuf: '0' quadrature: 'True' rfdc: 'True' samplerate: ' 1920000' type: fc32 uri: uri states: bus_sink: false bus_source: false bus_structure: null coordinate: [760, 236.0] rotation: 0 state: true - name: logpwrfft_x_0 id: logpwrfft_x parameters: affinity: '' alias: '' average: 'False' avg_alpha: '1.0' comment: '' fft_size: '1024' frame_rate: '30' maxoutbuf: '0' minoutbuf: '0' ref_scale: '2' sample_rate: samp_rate shift: 'False' type: complex states: bus_sink: false bus_source: false bus_structure: null coordinate: [1104, 224.0] rotation: 0 state: disabled - name: probSign id: blocks_probe_signal_x parameters: affinity: '' alias: '' comment: '' type: complex states: bus_sink: false bus_source: false bus_structure: null coordinate: [1080, 416.0] rotation: 0 state: enabled - name: probSign1 id: blocks_probe_signal_x parameters: affinity: '' alias: '' comment: '' type: complex states: bus_sink: false bus_source: false bus_structure: null coordinate: [520, 408.0] rotation: 0 state: disabled - name: python_mod id: epy_module parameters: alias: '' comment: '' source_code: "# this module will be imported in the into your flowgraph\nf1=2380000000\n\ f2=2420000000\nf=f1\nstep = 100000\n\ndef sweeper(prob_lvl):\n global f1,f2,f,step\n\ \ if prob_lvl:\n f +=step\n if f>f2:f=f1\n\n return f" states: bus_sink: false bus_source: false bus_structure: null coordinate: [848, 16.0] rotation: 0 state: true - name: qtgui_freq_sink_x_0 id: qtgui_freq_sink_x parameters: affinity: '' alias: '' alpha1: '1.0' alpha10: '1.0' alpha2: '1.0' alpha3: '1.0' alpha4: '1.0' alpha5: '1.0' alpha6: '1.0' alpha7: '1.0' alpha8: '1.0' alpha9: '1.0' autoscale: 'False' average: '1.0' axislabels: 'True' bw: samp_rate color1: '"blue"' color10: '"dark blue"' color2: '"red"' color3: '"green"' color4: '"black"' color5: '"cyan"' color6: '"magenta"' color7: '"yellow"' color8: '"dark red"' color9: '"dark green"' comment: '' ctrlpanel: 'True' fc: freq fftsize: '1024' freqhalf: 'True' grid: 'False' gui_hint: '' label: Relative Gain label1: '' label10: '''''' label2: '''''' label3: '''''' label4: '''''' label5: '''''' label6: '''''' label7: '''''' label8: '''''' label9: '''''' legend: 'True' maxoutbuf: '0' minoutbuf: '0' name: '""' nconnections: '1' norm_window: 'False' showports: 'False' tr_chan: '0' tr_level: '0.0' tr_mode: qtgui.TRIG_MODE_FREE tr_tag: '""' type: complex units: dB update_time: '0.10' width1: '1' width10: '1' width2: '1' width3: '1' width4: '1' width5: '1' width6: '1' width7: '1' width8: '1' width9: '1' wintype: window.WIN_BLACKMAN_hARRIS ymax: '10' ymin: '-140' states: bus_sink: false bus_source: false bus_structure: null coordinate: [1368, 188.0] rotation: 0 state: enabled - name: qtgui_time_sink_x_0 id: qtgui_time_sink_x parameters: affinity: '' alias: '' alpha1: '1.0' alpha10: '1.0' alpha2: '1.0' alpha3: '1.0' alpha4: '1.0' alpha5: '1.0' alpha6: '1.0' alpha7: '1.0' alpha8: '1.0' alpha9: '1.0' autoscale: 'False' axislabels: 'True' color1: blue color10: dark blue color2: red color3: green color4: black color5: cyan color6: magenta color7: yellow color8: dark red color9: dark green comment: '' ctrlpanel: 'False' entags: 'True' grid: 'False' gui_hint: '' label1: Signal 1 label10: Signal 10 label2: Signal 2 label3: Signal 3 label4: Signal 4 label5: Signal 5 label6: Signal 6 label7: Signal 7 label8: Signal 8 label9: Signal 9 legend: 'True' marker1: '-1' marker10: '-1' marker2: '-1' marker3: '-1' marker4: '-1' marker5: '-1' marker6: '-1' marker7: '-1' marker8: '-1' marker9: '-1' name: '""' nconnections: '1' size: '1024' srate: samp_rate stemplot: 'False' style1: '1' style10: '1' style2: '1' style3: '1' style4: '1' style5: '1' style6: '1' style7: '1' style8: '1' style9: '1' tr_chan: '0' tr_delay: '0' tr_level: '0.0' tr_mode: qtgui.TRIG_MODE_FREE tr_slope: qtgui.TRIG_SLOPE_POS tr_tag: '""' type: complex update_time: '0.10' width1: '1' width10: '1' width2: '1' width3: '1' width4: '1' width5: '1' width6: '1' width7: '1' width8: '1' width9: '1' ylabel: Amplitude ymax: '1' ymin: '-1' yunit: '""' states: bus_sink: false bus_source: false bus_structure: null coordinate: [520, 308.0] rotation: 0 state: disabled - name: qtgui_vector_sink_f_0 id: qtgui_vector_sink_f parameters: affinity: '' alias: '' alpha1: '1.0' alpha10: '1.0' alpha2: '1.0' alpha3: '1.0' alpha4: '1.0' alpha5: '1.0' alpha6: '1.0' alpha7: '1.0' alpha8: '1.0' alpha9: '1.0' autoscale: 'False' average: '1.0' color1: '"blue"' color10: '"dark blue"' color2: '"red"' color3: '"green"' color4: '"black"' color5: '"cyan"' color6: '"magenta"' color7: '"yellow"' color8: '"dark red"' color9: '"dark green"' comment: '' grid: 'False' gui_hint: '' label1: '' label10: '' label2: '' label3: '' label4: '' label5: '' label6: '' label7: '' label8: '' label9: '' maxoutbuf: '0' minoutbuf: '0' name: '""' nconnections: '1' ref_level: '0' showports: 'False' update_time: '0.10' vlen: '1024' width1: '1' width10: '1' width2: '1' width3: '1' width4: '1' width5: '1' width6: '1' width7: '1' width8: '1' width9: '1' x_axis_label: '"x-Axis"' x_start: '0' x_step: '1.0' x_units: '""' y_axis_label: '"y-Axis"' y_units: '""' ymax: '10' ymin: '-140' states: bus_sink: false bus_source: false bus_structure: null coordinate: [1384, 300.0] rotation: 0 state: disabled - name: uri id: parameter parameters: alias: '' comment: '' hide: none label: URI short_id: '' type: '' value: '"ip:192.168.2.1"' states: bus_sink: false bus_source: false bus_structure: null coordinate: [1000, 4.0] rotation: 0 state: enabled connections: - [analog_noise_source_x_0, '0', blocks_add_xx_0, '1'] - [analog_sig_source_x_0, '0', blocks_throttle_0, '0'] - [analog_sig_source_x_1, '0', blocks_add_xx_0, '0'] - [blocks_add_xx_0, '0', qtgui_freq_sink_x_0, '0'] - [blocks_throttle_0, '0', probSign1, '0'] - [blocks_throttle_0, '0', qtgui_time_sink_x_0, '0'] - [blocks_throttle_0_0, '0', logpwrfft_x_0, '0'] - [fft_vxx_0, '0', blocks_throttle_0_0, '0'] - [iio_pluto_source_0, '0', fft_vxx_0, '0'] - [iio_pluto_source_0, '0', probSign, '0'] - [iio_pluto_source_0, '0', qtgui_freq_sink_x_0, '0'] - [logpwrfft_x_0, '0', qtgui_vector_sink_f_0, '0'] metadata: file_format: 1
next is python_mod code
What is your dwell time requirement?
Note too that when you change frequency the data may not reflect the updated frequency as there is natural elasticity in the system. This delay would need to be measured.
-Travis
What is your dwell time requirement?
Note too that when you change frequency the data may not reflect the updated frequency as there is natural elasticity in the system. This delay would need to be measured.
-Travis
Kindly explain what do you mean by dwell time.
the user should be able to see the full spectrum of the sdr and the signal power for the frequency while it gets scanned and the scanning and display should be as fast as the capability of the sdr.
Please advise if this answers you queries to suggest a solution
Dwell time is how long you remain at one frequency.
-Travis
ok travis lets say 3 milli seconds that means the radio will be able to visit the same freq atlesst twict in a second for the bandwidth between 70 Mhz - 6 Ghz
Hope i am correct
Maybe I can frame this a bit for you. So in GNU Radio the way you are controlling frequency updates relative to the data stream is purely asynchronous. From the perspective of general software control of the LO frequency and data stream, they are asynchronous. This creates a scenarios like I mentioned in a previous post:
Note too that when you change frequency the data may not reflect the updated frequency as there is natural elasticity in the system. This delay would need to be measured
Without highly customizing the HDL and software control the only way to make sure the current data reflects the current desired frequency is to process say N buffers aka wait. N would take into account the GNU Radio inter-block buffers and the buffers libiio uses to stream data from hardware. By default the number of libiio buffers is 4 (size of buffers is set by the block). Getting the number of inline buffers in GNU Radio is complex since its managed by a scheduler. The hacky way to do this is to just make N large. Like >10+libiio buffers.
I would recommend verifying that your data reflects the desired frequency of interest. Say ping pong between 2 frequencies with known spectral content. Once that works you can scan the entire band of interest.
-Travis