Post Go back to editing

ABOUT the USB connector with the power mark on the ADALM2000

Category: Hardware
Product Number: ADALM2000

Please tell me how to use the USB connector with the power mark on the ADALM2000.

Can I connect a power adapter to this connector when the power supply capacity is insufficient?

  • That is correct as long as the adapter can supply enough current, 1 A should be minimum. The second USB connector is for supplying power to the device over-riding the power drawn from the host USB port (used for communications). This has two basic use cases. One, when using a non-powered USB hub and second for remote battery power when a wireless Wifi dongle is used for network communications with the device.