Hello everyone,
The setup:
I'm building the firmware for the Sidekiq Z2 using the ADI's plutosdr-fw repo. I'm working with the commit a1c2ce7 which is 5 commits ahead the v0.34 tag. In order to build it, I'm using the following commands:
export CROSS_COMPILE=arm-linux-gnueabihf-
export PATH=$PATH:/opt/Xilinx/SDK/2019.1/gnu/aarch32/lin/gcc-arm-linux-gnueabi/bin
export VIVADO_SETTINGS=/opt/Xilinx/Vivado/2019.1/settings64.sh
make TARGET=sidekiqz2
The build process runs smoothly, and I've not changed any functionality (in consecuence, the repo is as cloned) except from the line 119 of the makefile for:
make -C buildroot ARCH=arm zynq_$(TARGET)_vivado_2019_1_defconfig
As the 2019.1 Vivado version is what I use and have installed.
I've used the built firmware .dfu files for many weeks now, but I realized that something was wrong last week when I needed to access the 'config.txt' file in one of the boards that had the home-built firmware loaded and the file didn't exist.
The problem:
I am trying to solve the message "Bad FIT image format!" appearing when booting a Sidekiq Z2 with the firmware built by me. The boot logs are obtained by connecting the serial console and reseting the boards.
What strikes me as extremely odd, is that almost everything works, except for some specific features like the mounting of the filesystem for the USB drive (line 106 from the boot log attached), which prevents me from seeing the 'config.txt' file, necessary for my application. That is why I been using the custom builds for a while now without realizing about this error. It is worth mentioning that the FPGA transiever funcionality and most of the OS work fine, I've been ssh'ing to the board connected via USB whenever the OS was already up (obviously) and that is also the reason I've never got to see the "bad FIT image file format" message.
Also, the config.txt file exists and I can access it in /opt/config.txt, so I infer that the S40network script is working just fine.
I've also gone through the .dts files and various configuration files. Although I'm not an embedded linux building expert, I've some experience, but I can not see anything that stands out as strange. If you need the built firmware (.frm, .dfu) I'd be happy to give it to you.
I am really lost in this one, specially for this weird not-copmpletely-broken behaviour, so any help would be appreciated.
Below, I'm attaching the boot logs for both cases. Whenever I try to run S45msd inside the Linux, it just prints the same error messages that prints when booting.
Default firmware:
U-Boot PlutoSDR v0.20-PlutoSDR-00053-g89d07540f9 (Jan 23 2019 - 12:37:40 -0600), Build: jenkins-Sidekiq-sidekiq-z2-bsp-adi-2 I2C: ready DRAM: ECC disabled 512 MiB SF: Detected N25Q1024A with page size 256 Bytes, erase size 4 KiB, total 128 MiB In: serial@e0001000 Out: serial@e0001000 Err: serial@e0001000 Model: Zynq Sidekiq Z2 Board Hit any key to stop autoboot: 0 200 gpio: pin 48 (gpio 48) value is 1 Booting from QSPI Booting silently SF: Detected N25Q1024A with page size 256 Bytes, erase size 4 KiB, total 128 MiB device 0 offset 0x200000, size 0x9526b7 SF: 9774775 bytes @ 0x200000 Read: OK ## Checking Image at 02080000 ... FIT image found FIT description: Configuration to load fpga before Kernel Image 0 (fdt@1) Description: zynq-sidekiqz2 Type: Flat Device Tree Compression: uncompressed Data Start: 0x020800f4 Data Size: 20446 Bytes = 20 KiB Architecture: ARM Image 1 (fdt@2) Description: zynq-sidekiqz2-revb Type: Flat Device Tree Compression: uncompressed Data Start: 0x02085148 Data Size: 20446 Bytes = 20 KiB Architecture: ARM Image 2 (fdt@3) Description: zynq-sidekiqz2-revc Type: Flat Device Tree Compression: uncompressed Data Start: 0x0208a19c Data Size: 20446 Bytes = 20 KiB Architecture: ARM Image 3 (fpga@1) Description: FPGA Type: FPGA Image Compression: uncompressed Data Start: 0x0208f1e4 Data Size: 963140 Bytes = 940.6 KiB Load Address: 0x0f000000 Hash algo: md5 Hash value: 3bb49eefc2d7f579911746a0f11c0694 Image 4 (linux_kernel@1) Description: Linux Type: Kernel Image Compression: uncompressed Data Start: 0x0217a4e4 Data Size: 3459288 Bytes = 3.3 MiB Architecture: ARM OS: Linux Load Address: 0x00008000 Entry Point: 0x00008000 Hash algo: md5 Hash value: 31a3cb4322675a2e3ae7601474d830ee Image 5 (ramdisk@1) Description: Ramdisk Type: RAMDisk Image Compression: gzip compressed Data Start: 0x024c6e98 Data Size: 5287151 Bytes = 5 MiB Architecture: ARM OS: Linux Load Address: unavailable Entry Point: unavailable Hash algo: md5 Hash value: d0b4b27afe5e107f6a0fc0b3dc9031f7 Default Configuration: 'config@0' Configuration 0 (config@0) Description: Linux with fpga RevA Kernel: linux_kernel@1 Init Ramdisk: ramdisk@1 FDT: fdt@1 FPGA: fpga@1 Configuration 1 (config@1) Description: Linux with fpga RevB Kernel: linux_kernel@1 Init Ramdisk: ramdisk@1 FDT: fdt@2 FPGA: fpga@1 Configuration 2 (config@2) Description: Linux with fpga RevB Kernel: linux_kernel@1 Init Ramdisk: ramdisk@1 FDT: fdt@2 FPGA: fpga@1 Configuration 3 (config@3) Description: Linux with fpga RevB Kernel: linux_kernel@1 Init Ramdisk: ramdisk@1 FDT: fdt@2 FPGA: fpga@1 Configuration 4 (config@4) Description: Linux with fpga RevB Kernel: linux_kernel@1 Init Ramdisk: ramdisk@1 FDT: fdt@2 FPGA: fpga@1 Configuration 5 (config@5) Description: Linux with fpga RevB Kernel: linux_kernel@1 Init Ramdisk: ramdisk@1 FDT: fdt@2 FPGA: fpga@1 Configuration 6 (config@6) Description: Linux with fpga RevB Kernel: linux_kernel@1 Init Ramdisk: ramdisk@1 FDT: fdt@2 FPGA: fpga@1 Configuration 7 (config@7) Description: Linux with fpga RevB Kernel: linux_kernel@1 Init Ramdisk: ramdisk@1 FDT: fdt@2 FPGA: fpga@1 Configuration 8 (config@8) Description: Linux with fpga RevC Kernel: linux_kernel@1 Init Ramdisk: ramdisk@1 FDT: fdt@3 FPGA: fpga@1 Configuration 9 (config@9) Description: Linux with fpga RevB Kernel: linux_kernel@1 Init Ramdisk: ramdisk@1 FDT: fdt@2 FPGA: fpga@1 Configuration 10 (config@10) Description: Linux with fpga RevB Kernel: linux_kernel@1 Init Ramdisk: ramdisk@1 FDT: fdt@2 FPGA: fpga@1 ## Checking hash(es) for FIT Image at 02080000 ... Hash(es) for Image 0 (fdt@1): Hash(es) for Image 1 (fdt@2): Hash(es) for Image 2 (fdt@3): Hash(es) for Image 3 (fpga@1): md5+ Hash(es) for Image 4 (linux_kernel@1): md5+ Hash(es) for Image 5 (ramdisk@1): md5+ ## Loading kernel from FIT Image at 02080000 ... Using 'config@2' configuration Verifying Hash Integrity ... OK Trying 'linux_kernel@1' kernel subimage Description: Linux Type: Kernel Image Compression: uncompressed Data Start: 0x0217a4e4 Data Size: 3459288 Bytes = 3.3 MiB Architecture: ARM OS: Linux Load Address: 0x00008000 Entry Point: 0x00008000 Hash algo: md5 Hash value: 31a3cb4322675a2e3ae7601474d830ee Verifying Hash Integrity ... md5+ OK ## Loading ramdisk from FIT Image at 02080000 ... Using 'config@2' configuration Trying 'ramdisk@1' ramdisk subimage Description: Ramdisk Type: RAMDisk Image Compression: gzip compressed Data Start: 0x024c6e98 Data Size: 5287151 Bytes = 5 MiB Architecture: ARM OS: Linux Load Address: unavailable Entry Point: unavailable Hash algo: md5 Hash value: d0b4b27afe5e107f6a0fc0b3dc9031f7 Verifying Hash Integrity ... md5+ OK ## Loading fdt from FIT Image at 02080000 ... Using 'config@2' configuration Trying 'fdt@2' fdt subimage Description: zynq-sidekiqz2-revb Type: Flat Device Tree Compression: uncompressed Data Start: 0x02085148 Data Size: 20446 Bytes = 20 KiB Architecture: ARM Verifying Hash Integrity ... OK Booting using the fdt blob at 0x2085148 ## Loading fpga from FIT Image at 02080000 ... Trying 'fpga@1' fpga subimage Description: FPGA Type: FPGA Image Compression: uncompressed Data Start: 0x0208f1e4 Data Size: 963140 Bytes = 940.6 KiB Load Address: 0x0f000000 Hash algo: md5 Hash value: 3bb49eefc2d7f579911746a0f11c0694 Verifying Hash Integrity ... md5+ OK Loading fpga from 0x0208f1e4 to 0x0f000000 design filename = "system_top;UserID=0XFFFFFFFF;COMPRESS=TRUE;Version=2018.2" part number = "7z010clg225" date = "2019/01/23" time = "12:36:37" bytes in bitstream = 963020 zynq_align_dma_buffer: Align buffer at f000078 to f000000(swap 1) Programming full bitstream... OK Loading Kernel Image ... OK Loading Ramdisk to 1e61e000, end 1eb28cef ... OK Loading Device Tree to 1e616000, end 1e61dfdd ... OK Starting kernel ... Uncompressing Linux... done, booting the kernel. Starting logging: OK Starting mdev: OK Starting watchdog: OK Starting initializing random number generator: OK Starting miscellaneous setup: OK Starting UDC Gadgets: OK Starting system message bus: done Starting network: OK Starting dhcpd Daemon & httpd Server: OK Starting MSD Daemon: OK Starting dropbear sshd: OK Starting input-event-daemon: done Welcome to Sidekiq Z2 sidekiqz2 login:
Custom-built firmware:
U-Boot PlutoSDR v0.20-PlutoSDR-00065-ga2c2013a86 (Jul 27 2023 - 12:49:44 -0300) I2C: ready DRAM: ECC disabled 512 MiB SF: Detected N25Q1024A with page size 256 Bytes, erase size 4 KiB, total 128 MiB In: serial@e0001000 Out: serial@e0001000 Err: serial@e0001000 Model: Zynq Sidekiq Z2 Board Hit any key to stop autoboot: 0 205 gpio: pin 48 (gpio 48) value is 1 Booting from QSPI Booting silently SF: Detected N25Q1024A with page size 256 Bytes, erase size 4 KiB, total 128 MiB device 0 offset 0x200000, size 0x900000 SF: 9437184 bytes @ 0x200000 Read: OK ## Checking Image at 02080000 ... FIT image found Bad FIT image format! device 0 offset 0x200000, size 0x1e00000 SF: 31457280 bytes @ 0x200000 Read: OK ## Loading kernel from FIT Image at 02080000 ... Using 'config@2' configuration Verifying Hash Integrity ... OK Trying 'linux_kernel@1' kernel subimage Description: Linux Type: Kernel Image Compression: uncompressed Data Start: 0x0228d6fc Data Size: 3933080 Bytes = 3.8 MiB Architecture: ARM OS: Linux Load Address: 0x00008000 Entry Point: 0x00008000 Hash algo: md5 Hash value: 929d87a26671fe4c5a1d0e9262626608 Verifying Hash Integrity ... md5+ OK ## Loading ramdisk from FIT Image at 02080000 ... Using 'config@2' configuration Trying 'ramdisk@1' ramdisk subimage Description: Ramdisk Type: RAMDisk Image Compression: gzip compressed Data Start: 0x0264db70 Data Size: 18049519 Bytes = 17.2 MiB Architecture: ARM OS: Linux Load Address: unavailable Entry Point: unavailable Hash algo: md5 Hash value: 7ef612ea8d9a482e3881352716938027 Verifying Hash Integrity ... md5+ OK ## Loading fdt from FIT Image at 02080000 ... Using 'config@2' configuration Trying 'fdt@2' fdt subimage Description: zynq-sidekiqz2-revb Type: Flat Device Tree Compression: uncompressed Data Start: 0x02085964 Data Size: 22523 Bytes = 22 KiB Architecture: ARM Verifying Hash Integrity ... OK Booting using the fdt blob at 0x2085964 ## Loading fpga from FIT Image at 02080000 ... Trying 'fpga@1' fpga subimage Description: FPGA Type: FPGA Image Compression: uncompressed Data Start: 0x02090a38 Data Size: 2083846 Bytes = 2 MiB Load Address: 0x0f000000 Hash algo: md5 Hash value: b6a4a5eb709912af7a55ad5af52ffd53 Verifying Hash Integrity ... md5+ OK Loading fpga from 0x02090a38 to 0x0f000000 design filename = "system_top;UserID=0XFFFFFFFF;Version=2019.1" part number = "7z010clg225" date = "2022/11/09" time = "14:36:16" bytes in bitstream = 2083740 zynq_align_dma_buffer: Align buffer at f00006a to f000000(swap 1) Programming full bitstream... OK Loading Kernel Image ... OK Loading Ramdisk to 1d9f3000, end 1eb299ef ... OK Loading Device Tree to 1d9ea000, end 1d9f27fa ... OK Starting kernel ... gpio gpiochip0: (zynq_gpio): gpiochip_lock_as_irq: tried to flag a GPIO set as output for IRQ gpio gpiochip0: (zynq_gpio): unable to lock HW IRQ 14 for IRQ genirq: Failed to request resources for Button (irq 57) on irqchip zynq-gpio gpio-keys gpio_keys: Unable to claim irq 57; error -5 Starting syslogd: OK Starting klogd: OK Running sysctl: OK Starting mdev: OK Starting watchdog: OK Starting initializing random number generator: OK Starting miscellaneous setup: OK Starting UDC Gadgets: OK Starting system message bus: done Starting network: OK Starting dhcpd Daemon & httpd Server: OK Starting MSD Daemon: mount: mounting /dev/loop7 on /mnt/msd failed: No such file or directory md5sum: can't open '/mnt/msd/config.txt': Not a directory cp: can't stat '/mnt/msd/img': Not a directory cp: can't stat '/mnt/msd/index.html': Not a directory mv: can't stat '/mnt/msd/info.html': Not a directory umount: can't unmount /mnt/msd: Invalid argument OK Starting dropbear sshd: OK Starting input-event-daemon: input-event-daemon: open(/dev/input/event0): No such file or directory done Welcome to Sidekiq Z2 sidekiqz2 login:
Thanks in advance.
I am trying to solve the message "Bad FIT image format!" appearing when booting a Sidekiq Z2 with the firmware built by me. The boot logs are obtained by connecting the serial console and reseting the boards.
These two things are unrelated.
The Bad FIT image format, comes from the fact that the fit_size uboot variable is not set correctly.
In this case the u-boot script will do a SF read of the entire SPI flash to the end.
In case this wouldn't work you would not boot into Linux.
Regarding the msd issue, I would start debugging here:
https://github.com/analogdevicesinc/buildroot/blob/master/board/pluto/post-build.sh#L39
The original vfat image is created on the build host. Maybe it's not working on your end?
-Michael
Thanks for your response Michael,
These two things are unrelated.
This will help me target the issues separately.
The Bad FIT image format, comes from the fact that the fit_size uboot variable is not set correctly.
I see. This leads to another question that is: why could this be happening?
I see that the u-boot default enviroment declares fit_size as 0x900000 in 'u-boot-xlnx/include/configs/zynq_zc70x_sidekiqz2.h'. From my understanding this number should be alright or automatically updated.
I've some reference firmware that works correctly and I've compared the FIT files with hexdumps and strings and at least the uboot-env.dfu is identical (the fit_size is set as default as 0x900000).
What I couldn't do is find out where the fit_size is set to the correct value in the u-boot environment.
Should I look for something else? Should I change the value manually? (The second one I don't think)
The original vfat image is created on the build host. Maybe it's not working on your end?
I'll take a look and ask here again if I reach a dead end.
This is beyond helpful, thanks again.
fit_size is set by the srcipt that handles the FRM files on the MSD:
fit_size is also set when doing DFU SF:
If it wasn't set before it defaults:
-Michael
Hello Michael,
I've been doing some research these few days about the vfat image generation and the mounting process in different versions.
In case someone has the same problem, here is the solution:
In this commit the mount points have changed for Pluto and m2k. The thing is that some Pluto scripts are used directly by the Sidekiq Z2, but under /board/sidekiqz2/device_config and /board/sidekiqz2/post-build.sh, the mounting point for the Sidekiq Z2 has not yet been updated.
The solution I've found is to manually edit both device_config and post-build.sh with the proper mounting points.
Should I post an issue in the repo?
Thanks,
Best.
Should I post an issue in the repo?
Yes, please create an issue. So that this doesn't get lost.
I'll fix this for the next release which I draft in approx 3 weeks from now.
-Michael