Post Go back to editing
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

ADALM-PLUTO maximum frequency

Category: Hardware
Product Number: ADALM-PLUTO

Hi, 

we are running a project which need the ADALM-PLUTO with default AD9363 to operation around 6GHz. we need suggest on the following solutions, which one is better?

1) using the U-Boot's fw_printenv and fw_setenv commands to get that device's larger tuning range (70-6000 MHz) and larger bandwidth (56MHz).

2) de-soldering the AD9363 and replace with AD9361. 

Or, is there a ADALM-PLUTO module with AD9361 we can purchase? 

Thank you




[locked by: travisfcollins at 3:34 PM (GMT -4) on 5 Jun 2023]