Post Go back to editing

about the transient response experiment example of RL Circuit using adalm2000

Category: Hardware
Software Version: scopy:1.4.1

In the transient response experiment example of RL Circuit using adalm2000 in the following URL, 4V peak-peak voltage is used as input (W1).
But why is it measuring about 3V peak-peak voltage on channel 1 (the voltage across the entire circuit)?
wiki.analog.com/.../rl_transient_response