Post Go back to editing

PDM convert to analog

Dear Sir or Madam,

in my studies I am working on a project to measure 2 microphones.

For this purpose a small sound absorber chamber is built to measure with
measurement electronics an analog reference microphone (the b&k 4165) and a DUT
(e.g. the digital microphone Infineon IM69D130-DS).

We used the 4165 mic as well as a suitable preamp and the FFT
Analyzer 3160 from the company B&K.

The FFT Analyzer requires analog signals at the input and converts them to
digital signals with a sampling rate of 131kHz.

My problem is to pick up the digital microphone IM69D130-DS. This
MEMS micro gives as signal a 1-bit PDM signal, which I have to convert to an
analog signal, so that the FFT Analyzer recognizes it.

Do you offer such an interface or chip that turns a PDM signal into an analog one?

kind regards



tag
[edited by: lallison at 10:44 PM (GMT -5) on 31 Jan 2023]
Parents
  • I think the closest thing to a single PDM to "analog" output chip we offer is one or another of these kind of PDM to class D audio amplifiers from our Maxim parts:

    https://datasheets.maximintegrated.com/en/ds/MAX98358.pdf

    The output will be way bigger / more power than you need to send to the analyzer and will need to be filtered to remove the class D clock switching but with little or now output load and heavy anti-aliasing filter it might have low enough distortion.

    There are others in the catalog so do a search to see them all and check the data sheets to see it they might be a fit for your needs.

Reply
  • I think the closest thing to a single PDM to "analog" output chip we offer is one or another of these kind of PDM to class D audio amplifiers from our Maxim parts:

    https://datasheets.maximintegrated.com/en/ds/MAX98358.pdf

    The output will be way bigger / more power than you need to send to the analyzer and will need to be filtered to remove the class D clock switching but with little or now output load and heavy anti-aliasing filter it might have low enough distortion.

    There are others in the catalog so do a search to see them all and check the data sheets to see it they might be a fit for your needs.

Children