Hello everyone.
I would like to ask a question about the transmission of baseband signals using ADALM-*** SDR.
I need to send a baseband OFDM signal using the SMA cable to a visible light communication set. In this case I need my signal to work between 0 and 5MHz. I even read in the documentation that it is possible to transmit and receive signals in baseband using ADALM PLUTO but using the internal loopback path of the AD9363.
I always see people working with the passband signal on the SMA output and the Mathworks documentation says that a carrier center frequency is needed to form the output signal.
I would like to ask if it is possible to deliver the baseband signal to the SMA connector and work with it at the output of the ADALM PLUTO.
In other words, I would like to know if it is possible to bypass the RF Front End circuit and output the baseband signal to the SMA output connector.
Best Regards
[locked by: travisfcollins at 11:11 PM (GMT -4) on 29 Mar 2022]