Hello,
currently I'm trying to send bursts using FSK by following the FSK Receiver and FSK Transmitter templates on the GNURadio Github. When I use the ZMQ Blocks to test the flowgraph it works just fine (meaning: a packet is printed out every 500ms), but when I use the PlutoSDR to receive and transmit there is a lot of packet loss (meaning: a packet is printed out every ~4000ms). Is there a way to set the PlutoSDRs parameters to to be better suite the task? or is that amount of packet loss to be expected?
Thanks in advance, any hints/solutions are highly appreciated.
Best,
Ottega