Post Go back to editing

Is it possible to external trigger ADALM2000 function generator outputs?

Hello,

In one of my project I need to generate two waveforms(W1 and W2) with some phase delays.

W1 will be a staircase increasing sawtooth waveform. 

W2 will be a pulse train with N number of pulses.

I can generate these signals in Scopy but I want them to start with an external trigger because I need them to be in sync with another system.

So each time external trigger input's rising edge W1 and W2 will generate a waveform(one pulse train and one staircase sawtooth) and stop. 

Is such triggering possible using ADALM2000? I would appreciate any help,