Post Go back to editing

ADALM2000 does not start under Windows 10 after installation

Hi,

I followed the installation steps and Scopy does not start after installation under Windows.

In another Windows it starts but completely blocks the internet. I am super frustrated.

Please I need help! 

Parents Reply
  • It seems I solved the first issue myself. 

    Here what I did:

    Eventlog of Windows was showing an issue with libusb-1.0.dll.

    Scopy was installed in: C:\Program Files\Analog Devices\Scopy

    I downladed the latest verison of libusb-1.0.dll here https://libusb.info/

    Then I copied libusb-1.0.dll into Scopy folder and overwrote the existing one. So far it works. 

     

    So the next issue is with the other PC where Scopy blocks internet when USB is plugged in.

Children
  • The internet blocking may be related to phonehome feature of Scopy (it checks if scopy needs to be updated). It could be your firewall that's acting up. Either allow Scopy to access the internet, or go to Scopy preferences, and uncheck "Enable automatic update checking". 

    Besides this feature, Scopy does not access the internet in any way.

    -Adrian

  • Another issue may be related to the fact that the ADALM2000 creates a virtual ethernet device when plugged in, check out mhennerich response up in the thread.

  • Hi,

    Both didn't work for me. Its happening before I open Scopy.

    Here I am going the write details without private info. I hope you or some support people here can help me.

    So the issue happens when I plug ADALM2000 right after it pops up the ADALM2000 drive. 

    Here is my config file:

    [NETWORK]
    hostname = m2k
    ipaddr = 192.168.4.1
    ipaddr_host = 192.168.4.10
    netmask = 255.255.255.0

    [WLAN]
    ssid_wlan =
    pwd_wlan =
    ipaddr_wlan =

    [USB_ETHERNET]
    ipaddr_eth =
    netmask_eth = 255.255.255.0

    [SYSTEM]
    xo_correction =
    udc_handle_suspend = 0
    # USB Communication Device Class Compatibility Mode [rndis|ncm|ecm]
    usb_ethernet_mode = 0

    [ACTIONS]
    diagnostic_report = 0
    dfu = 0
    reset = 0
    calibrate = 0

    Here is the network situation before ADALM2000 is connected:


    Wireless LAN adapter Local Area Connection* 3:

    Media State . . . . . . . . . . . : Media disconnected
    Connection-specific DNS Suffix . :

    Wireless LAN adapter Local Area Connection* 4:

    Media State . . . . . . . . . . . : Media disconnected
    Connection-specific DNS Suffix . :

    Wireless LAN adapter Wi-Fi:

    Connection-specific DNS Suffix . :
    Link-local IPv6 Address . . . . . : fe80::1997:7a44:fded:cb05%7
    IPv4 Address. . . . . . . . . . . : 10.209.196.138
    Subnet Mask . . . . . . . . . . . : 255.255.128.0
    Default Gateway . . . . . . . . . : 10.209.128.1

    Here is the network situation after ADALM2000 is connected:

    Ethernet adapter Ethernet 2:

    Connection-specific DNS Suffix . :
    Link-local IPv6 Address . . . . . : fe80::15e3:e73b:7426:a862%17
    IPv4 Address. . . . . . . . . . . : 192.168.4.10
    Subnet Mask . . . . . . . . . . . : 255.255.255.0
    Default Gateway . . . . . . . . . :

    Wireless LAN adapter Local Area Connection* 3:

    Media State . . . . . . . . . . . : Media disconnected
    Connection-specific DNS Suffix . :

    Wireless LAN adapter Local Area Connection* 4:

    Media State . . . . . . . . . . . : Media disconnected
    Connection-specific DNS Suffix . :

    Wireless LAN adapter Wi-Fi:

    Media State . . . . . . . . . . . : Media disconnected
    Connection-specific DNS Suffix . :

    As you see above IPv4 address of Wireless LAN is 10.209.196.138 and ADALM2000 has 192.168.4.10. And when I plug the USB of the ADALM2000 it creates virtual Ethernet but disconnects the Wifi. Disabling and enabling them also didn't work.

    I have been struggling with this years.

  • It didnt work. I followed the exact steps:

    1. Open Registry Editor.

    2. Go to HKEY_LOCAL_MACHINE\Software\Policies\Microsoft\Windows\WcmSvc\Local.

    3. Create/change the fMinimizeConnections registry DWORD to 0.

    4. Close Registry Editor and reboot.

    Still ADALM2000 blocks the Wifi adapter in two PCs.