Hi,
I followed the installation steps and Scopy does not start after installation under Windows.
In another Windows it starts but completely blocks the internet. I am super frustrated.
Please I need help!
Hi,
I followed the installation steps and Scopy does not start after installation under Windows.
In another Windows it starts but completely blocks the internet. I am super frustrated.
Please I need help!
I followed the installation steps and Scopy does not start after installation under Windows.
Can you please provide more information. Does it crash or hang? Can you start Scopy without ADALM2000 connected?
In another Windows it starts but completely blocks the internet.
You say - once you connect ADALM2000 to your PC USB (without starting Scopy), your network becomes unresponsive?
What subnet is your PC using for internet? 192.168.2.x ?
If that's the case, follow the instruction here:
https://wiki.analog.com/university/tools/pluto/users/customizing#multiple_devices
And try following:
ipaddr = 192.168.4.1
ipaddr_host = 192.168.4.10
-Michael
HI, thanks for getting back. I really need urgent help with this.
Lets first focus on Scopy not being started in my PC.
Yes Scopy tries to open and closes automatically in a millisecond. This happens regardless of ADALM2000 is connected. And after my installation it doesnt create ADI folder under roaming as well.
I can send the dmp file if you need.
Yes please provide your dump file.
ScopyCrashDump--2022-01-24--15-57-03.zip
Latest dmp files
Meanwhile I tried your suggestion(ipaddr ipaddr_host changes on the other PC(internet blocking issue), it didnt work. But lets look at it after we can solve the first one(Scopy exiting immediately after start). Because it is more critical. Im using the latest firmware and SW and drivers ect. And the internet blocking issue always exsited. I could live with that. But now in one of my PC Scopy does not even start.
Both machines are 64 bit Windows. I cant believe such critical issues exists in both PCs.