Post Go back to editing

Upgrade GNURADIO on ADRV9361-Z7035+ADRV1CRR-BOB

Hi,

I have developed, with succecs, some code in GNUradio on a client PC with UBUNTU where I have installed gr3.8 gr-iio and others tools and modules.

During my developing, I have started iiod deamon on ADRV9361-Z7035+ADRV1CRR-BOB, and read data on PC (Ethernet).

Now I need to migrate my code, without graphics (I will create only the python code) on ADRV9361-Z7035+ADRV1CRR-BOB and use

the ZMQ blocks of GNUradio to connect with the GUI on the client PC.

The problem is that the GNUradio on ADRV9361-Z7035+ADRV1CRR-BOB is version 3.7. This version don't include ZMQ. Also the implementation of GR-IIO

are different from the version tha I have installed on UBUNTU (I follow the wiki that suggest 3.8). For example FMComms2 output are I-Q float vs. complex in 3.8.

Any suggestions?