Post Go back to editing

Pattern Generator Library in Python for ADALM2000 / libm2k

Is there any python package for pattern generator as available in Scopy. 

I want to use the clock generator and pulse generator functions in parallel with the SPI functionality.

I see that there is a C++ library available scopy/src/patterngenerator at master · analogdevicesinc/scopy (github.com)

Parents Reply
  • Hello, 

    there seems to be some issues with the changes implemented. I have installed the library from the artifact links. However, my original code with spi_write_and_read() funciton is not working.

    First time, when I do a spi write, it works as it is only a write command and there is no readback expected.. But when I repeat the same statement again, it is stuck waiting for some response. 

Children