Post Go back to editing

Pattern Generator Library in Python for ADALM2000 / libm2k

Is there any python package for pattern generator as available in Scopy. 

I want to use the clock generator and pulse generator functions in parallel with the SPI functionality.

I see that there is a C++ library available scopy/src/patterngenerator at master · analogdevicesinc/scopy (github.com)

Parents Reply
  • Clock and Pulse features have to be concurrent with the SPI pattern, but not necessary as the same SPI SCLK rate. 

    I see that I can do that in Scopy. But I need to automate all the tasks and hence want to use the functionality in Python.

    Is there a possibility of extracting the digital pattern from the SPI functionality and join them with the Clock and Pulse features, if I have to write codes.

    Also, there are some "extra" parameters with spi_init but with no documentation. Can you please let me know what they are and how they can be used.

Children