ADALM-PLUTO firmware update fails

*** happens! I unplugged the usb-connection while pluto was updating firmware (LED1 flashed fast)! Now no usb-connection is available. Is there a way to reset the pluto?

Thanks Andreas

Top Replies

Parents Reply
  • there are no diff's Frowning2(I did not changed any of the hardware.) 

    But after I changend the config ip-address in the runing device (the new one): It also behaves as the other one: No connection: all Ports are filtered.

    this is my config file:

    # Analog Devices PlutoSDR Rev.B (Z7010-AD9363)
    # Device Configuration File
    #   1. Open with an Editor
    #   2. Edit this file
    #   3. Save this file on the device USB drive
    #   4. Eject the device USB Drive
    # Doc: https://wiki.analog.com/university/tools/pluto/users/customizing
    
    [NETWORK]
    hostname = pluto
    ipaddr = 192.168.1.114
    ipaddr_host = 192.168.1.115
    netmask = 255.255.255.0
    
    [WLAN]
    ssid_wlan = 
    pwd_wlan = 
    ipaddr_wlan = 
    
    [USB_ETHERNET]
    ipaddr_eth = 192.168.1.116
    netmask_eth = 255.255.255.0
    
    [SYSTEM]
    xo_correction = 
    udc_handle_suspend = 0
    # USB Communication Device Class Compatibility Mode [rndis|ncm|ecm]
    usb_ethernet_mode = 0
    
    [ACTIONS]
    diagnostic_report = 0
    dfu = 0
    reset = 0
    calibrate = 0
    

Children