ADALM-PLUTO firmware update fails

*** happens! I unplugged the usb-connection while pluto was updating firmware (LED1 flashed fast)! Now no usb-connection is available. Is there a way to reset the pluto?

Thanks Andreas

Top Replies

Parents Reply
  • 0
    •  Analog Employees 
    on Apr 30, 2021 6:18 AM in reply to HB9HCI

    Works for me -

    Starting Nmap 7.80 ( https://nmap.org ) at 2021-04-30 08:18 CEST
    Nmap scan report for pluto.local (10.44.3.53)
    Host is up (0.0020s latency).
    Not shown: 998 closed ports
    PORT   STATE SERVICE
    22/tcp open  ssh
    80/tcp open  http
    
    Nmap done: 1 IP address (1 host up) scanned in 0.22 seconds
    

    -Michael

Children