Post Go back to editing

Driving ADALM-PLUTO SDR from Android

Hi, I have an ADALM Pluto SDR. I have configured it for USB-Ethernet communications, and plan to connect an Android device to the SDR, and write software to drive the radio.


But, I'm wondering how I can drive lib_iio operations on the radio? I have seen the instructions about installing drivers on windows/mac/linux. However, since I can not do this on Android (I assume), what are my options? The only avenue I can think of is to open an SSH session on the radio and remotely execute iio operations. e.g. I did this and ran `iio_info -s` to get the library versions.

Is this a viable option, or is there a more direct approach via USB? Or perhaps there's a REST API?