tADALM-PLUTO boots, ssh works but no data, software recognizes but won't tune.

The Pluto boots, allows logon through ssh and populates as a mass storage device. That's where any functionality ends. The IIO_Oscilloscope program recognizes the device but no channels populate and two warning triangles appear in the toolbar. The various fields under DMM in that application do function and fluctuate in what seems to be a normal manner. There are two devices available to capture data from and a sample of the measurements is below.

adm1177:current0 = 243.319336 Milliampere
adm1177:voltage0 = 5.069287 Volts
xadc:temp0 = 48.97 °C
xadc:vccaux = 1.793701 Volts
xadc:vccbram = 1.007812 Volts
xadc:vccint = 1.009277 Volts
xadc:vccoddr = 1.342529 Volts
xadc:vccpaux = 1.795166 Volts
xadc:vccpint = 1.004883 Volts
xadc:voltage8 = 0.895996 Volts
xadc:vrefn = 0.000000 Volts
xadc:vrefp = 1.250244 Volts

SDRAngel on Linux recognizes the device but once it's selected and capture button clicked, the frequency is locked at 9,999,999 with nothing in the spectrum or waterfall. The console is a bit more enlightening:

2020-10-15 15:42:46.056 (I) WebAPIServer::start: starting web API server at http://127.0.0.1:8091
2020-10-15 15:44:41.547 (C) PlutoSDRInput::openDevice: cannot open Rx channel
2020-10-15 15:44:41.547 (C) PlutoSDRInput::PlutoSDRInput: cannot open device
2020-10-15 15:44:41.557 (C) PlutoSDRInput::applySettings: device not open
2020-10-15 15:44:41.654 (C) PlutoSDRInput::applySettings: device not open
2020-10-15 15:44:43.454 (C) PlutoSDRInput::applySettings: device not open
2020-10-15 15:44:43.455 (W) PlutoSDRInputThread::run: error refilling buf (1) 0 / 32768
2020-10-15 15:44:43.655 (W) PlutoSDRInputThread::run: error refilling buf (1) 0 / 32768
(...This continues a while...)

The output of iio_info -s

Library version: 0.21 (git tag: v0.21)
Compiled with backends: local xml ip usb serial
Unable to create Local IIO context : No such file or directory
Available contexts:
    0: 0456:b673 (Analog Devices Inc. PlutoSDR (ADALM-PLUTO)), serial=1044739659930006080031003fdc278679 [usb:2.19.5]

Up until 20 minutes ago, there were actually two contexts with the second being the expected ip: uri (ip:192.168.2.1). SSH is still up at that address. Rebooted the Pluto, still only showing the usb context. Either way, the main issue is the same.

Moved it over to the W10 machine and ran SDR-Console.

"One or more devices not found. This device did not start properly, possibly due to insufficient USB power. Reset the device and try again."

Ok, for giggles I unplugged it, plugged in a USB power supply to the right port and then the USB to the laptop. Same message.

SDRAngel on W10: Exact same issue, but no console for this one.

IIO_Oscilloscope on W10: Same but without the warning triangles. No channels available, clicking the capture (play?) button crashes the program.

The output of iio_info -u ip:192.168.2.1 (Yes, this somehow works even though, now, the ip context is no longer being listed.)

[16:31:32]root@SoRad-M:~# iio_info -u ip:192.168.2.1
Library version: 0.21 (git tag: v0.21)
Compiled with backends: local xml ip usb serial
IIO context created with network backend.
Backend version: 0.18 (git tag: v0.18  )
Backend description string: 192.168.2.1 Linux (none) 4.14.0-42540-g387d584 #301 SMP PREEMPT Wed Jul 3 15:06:53 CEST 2019 armv7l
IIO context has 9 attributes:
    hw_model: Analog Devices PlutoSDR Rev.B (Z7010-)
    hw_model_variant: 0
    hw_serial: 1044739659930006080031003fdc278679
    fw_version: v0.31
    ad9361-phy,xo_correction:
    ad9361-phy,model:
    local,kernel: 4.14.0-42540-g387d584
    ip,ip-addr: 192.168.2.1
    uri: ip:192.168.2.1
IIO context has 2 devices:
    iio:device0: adm1177
        2 channels found:
            voltage0:  (input)
            2 channel-specific attributes found:
                attr  0: raw value: 782
                attr  1: scale value: 6.433105468
            current0:  (input)
            2 channel-specific attributes found:
                attr  0: raw value: 445
                attr  1: scale value: 0.516601562
        No trigger on this device
    iio:device1: xadc
        10 channels found:
            voltage5: vccoddr (input)
            2 channel-specific attributes found:
                attr  0: raw value: 1833
                attr  1: scale value: 0.732421875
            voltage0: vccint (input)
            2 channel-specific attributes found:
                attr  0: raw value: 1378
                attr  1: scale value: 0.732421875
            voltage4: vccpaux (input)
            2 channel-specific attributes found:
                attr  0: raw value: 2445
                attr  1: scale value: 0.732421875
            temp0:  (input)
            3 channel-specific attributes found:
                attr  0: offset value: -2219
                attr  1: raw value: 2611
                attr  2: scale value: 123.040771484
            voltage7: vrefn (input)
            2 channel-specific attributes found:
                attr  0: raw value: 1
                attr  1: scale value: 0.732421875
            voltage1: vccaux (input)
            2 channel-specific attributes found:
                attr  0: raw value: 2451
                attr  1: scale value: 0.732421875
            voltage2: vccbram (input)
            2 channel-specific attributes found:
                attr  0: raw value: 1375
                attr  1: scale value: 0.732421875
            voltage3: vccpint (input)
            2 channel-specific attributes found:
                attr  0: raw value: 1371
                attr  1: scale value: 0.732421875
            voltage8:  (input)
            2 channel-specific attributes found:
                attr  0: raw value: 3672
                attr  1: scale value: 0.244140625
            voltage6: vrefp (input)
            2 channel-specific attributes found:
                attr  0: raw value: 1704
                attr  1: scale value: 0.732421875
        1 device-specific attributes found:
                attr  0: sampling_frequency value: 961538
        No trigger on this device
[16:38:53]root@SoRad-M:~# iio_attr -u ip:192.168.2.1 -C
IIO context with 9 attributes:
hw_model: Analog Devices PlutoSDR Rev.B (Z7010-)
hw_model_variant: 0
hw_serial: 1044739659930006080031003fdc278679
fw_version: v0.31
ad9361-phy,xo_correction:
ad9361-phy,model:
local,kernel: 4.14.0-42540-g387d584
ip,ip-addr: 192.168.2.1
uri: ip:192.168.2.1
 

I can also provide the output dmesg.

To make a long story short: There's definitely something wrong with this device but lacking anything to compare my results with (though I vaugely recall there being some logs posted that suggest I'm missing a device initialization in here somewhere) and no errors being thrown on the device itself I'm leaning toward this being an issue with the hardware itself.

Any suggestions or where do I mail this for a replacement (it was purchased from Mouser)?

(I originally updated the firmware from the .31 that shipped to .32. I have since downgraded to .31 in an attempt to resolve the issue but there has been no change, other than .32 having an unrelated error loading the 802.11 regulatory database that .31 does not have.)

Parents
  • No, it's brand new, haven't opened the case or tried any third party firmware, and it has been doing this since I first plugged it in (Well, after I finally convinced my linux machine to stop assigning 192.168.7.XX to the usb-ethernet interface, but that's another story.)

    login as: root
    root@192.168.2.1's password:
    Welcome to:
    ______ _       _        _________________
    | ___ \ |     | |      /  ___|  _  \ ___ \
    | |_/ / |_   _| |_ ___ \ `--.| | | | |_/ /
    |  __/| | | | | __/ _ \ `--. \ | | |    /
    | |   | | |_| | || (_) /\__/ / |/ /| |\ \
    \_|   |_|\__,_|\__\___/\____/|___/ \_| \_|
    
    v0.31
    http://wiki.analog.com/university/tools/pluto
    # dmesg
    Booting Linux on physical CPU 0x0
    Linux version 4.14.0-42540-g387d584 (michael@mhenneri-D06) (gcc version 7.2.1 20171011 (Linaro GCC 7.2-2017.11-rc1)) #301 SMP PREEMPT Wed Jul 3 15:06:53 CEST 2019
    CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
    CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
    OF: fdt: Machine model: Analog Devices PlutoSDR Rev.B (Z7010/AD9363)
    Memory policy: Data cache writealloc
    cma: Reserved 256 MiB at 0x0e400000
    On node 0 totalpages: 131072
    free_area_init_node: node 0, pgdat c093bf00, node_mem_map dfb77000
      Normal zone: 1024 pages used for memmap
      Normal zone: 0 pages reserved
      Normal zone: 131072 pages, LIFO batch:31
    random: fast init done
    percpu: Embedded 16 pages/cpu @dfb4b000 s32972 r8192 d24372 u65536
    pcpu-alloc: s32972 r8192 d24372 u65536 alloc=16*4096
    pcpu-alloc: [0] 0 [0] 1
    Built 1 zonelists, mobility grouping on.  Total pages: 130048
    Kernel command line: console=ttyPS0,115200 maxcpus=1 rootfstype=ramfs root=/dev/ram0 rw quiet loglevel=4 uboot=U-Boot PlutoSDR v0.20-PlutoSDR-00053-g89d0754 (Jan 14 2019 - 13:15:56 +0100)
    PID hash table entries: 2048 (order: 1, 8192 bytes)
    Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
    Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
    Memory: 242260K/524288K available (5120K kernel code, 243K rwdata, 1288K rodata, 1024K init, 151K bss, 19884K reserved, 262144K cma-reserved, 0K highmem)
    Virtual kernel memory layout:
        vector  : 0xffff0000 - 0xffff1000   (   4 kB)
        fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
        vmalloc : 0xe0800000 - 0xff800000   ( 496 MB)
        lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
        pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
        modules : 0xbf000000 - 0xbfe00000   (  14 MB)
          .text : 0xc0008000 - 0xc0600000   (6112 kB)
          .init : 0xc0800000 - 0xc0900000   (1024 kB)
          .data : 0xc0900000 - 0xc093cde0   ( 244 kB)
           .bss : 0xc0940ec0 - 0xc0966af4   ( 152 kB)
    Preemptible hierarchical RCU implementation.
            RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
            Tasks RCU enabled.
    RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
    NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
    efuse mapped to e0800000
    slcr mapped to e0802000
    L2C: platform modifies aux control register: 0x72360000 -> 0x72760000
    L2C: DT/platform modifies aux control register: 0x72360000 -> 0x72760000
    L2C-310 erratum 769419 enabled
    L2C-310 enabling early BRESP for Cortex-A9
    L2C-310 full line of zeros enabled for Cortex-A9
    L2C-310 ID prefetch enabled, offset 1 lines
    L2C-310 dynamic clock gating enabled, standby mode enabled
    L2C-310 cache controller enabled, 8 ways, 512 kB
    L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76760001
    zynq_clock_init: clkc starts at e0802100
    Zynq clock init
    sched_clock: 64 bits at 333MHz, resolution 3ns, wraps every 4398046511103ns
    clocksource: arm_global_timer: mask: 0xffffffffffffffff max_cycles: 0x4ce07af025, max_idle_ns: 440795209040 ns
    Switching to timer-based delay loop, resolution 3ns
    clocksource: ttc_clocksource: mask: 0xffff max_cycles: 0xffff, max_idle_ns: 537538477 ns
    timer #0 at e080a000, irq=17
    Console: colour dummy device 80x30
    Calibrating delay loop (skipped), value calculated using timer frequency.. 666.66 BogoMIPS (lpj=3333333)
    pid_max: default: 32768 minimum: 301
    Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
    Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
    CPU: Testing write buffer coherency: ok
    CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
    Setting up static identity map for 0x100000 - 0x100060
    Hierarchical SRCU implementation.
    smp: Bringing up secondary CPUs ...
    smp: Brought up 1 node, 1 CPU
    SMP: Total of 1 processors activated (666.66 BogoMIPS).
    CPU: All CPU(s) started in SVC mode.
    devtmpfs: initialized
    VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
    clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
    futex hash table entries: 512 (order: 3, 32768 bytes)
    pinctrl core: initialized pinctrl subsystem
    NET: Registered protocol family 16
    DMA: preallocated 256 KiB pool for atomic coherent allocations
    cpuidle: using governor ladder
    hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
    hw-breakpoint: maximum watchpoint size is 4 bytes.
    zynq-ocm f800c000.ocmc: ZYNQ OCM pool: 256 KiB @ 0xe0840000
    zynq-pinctrl 700.pinctrl: zynq pinctrl initialized
    e0001000.serial: ttyPS0 at MMIO 0xe0001000 (irq = 25, base_baud = 6249999) is a xuartps
    console [ttyPS0] enabled
    SCSI subsystem initialized
    usbcore: registered new interface driver usbfs
    usbcore: registered new interface driver hub
    usbcore: registered new device driver usb
    FPGA manager framework
    clocksource: Switched to clocksource arm_global_timer
    NET: Registered protocol family 2
    TCP established hash table entries: 4096 (order: 2, 16384 bytes)
    TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
    TCP: Hash tables configured (established 4096 bind 4096)
    UDP hash table entries: 256 (order: 1, 8192 bytes)
    UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
    NET: Registered protocol family 1
    Trying to unpack rootfs image as initramfs...
    Freeing initrd memory: 5540K
    hw perfevents: no interrupt-affinity property for /pmu@f8891000, guessing.
    hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
    workingset: timestamp_bits=30 max_order=17 bucket_order=0
    io scheduler noop registered
    io scheduler deadline registered
    io scheduler cfq registered (default)
    io scheduler mq-deadline registered
    io scheduler kyber registered
    brd: module loaded
    loop: module loaded
    m25p80 spi1.0: SPI-NOR-UniqueID 1044739659930006080031003fdc278679
    m25p80 spi1.0: n25q256a (32768 Kbytes)
    4 ofpart partitions found on MTD device spi1.0
    Creating 4 MTD partitions on "spi1.0":
    0x000000000000-0x000000100000 : "qspi-fsbl-uboot"
    0x000000100000-0x000000120000 : "qspi-uboot-env"
    0x000000120000-0x000000200000 : "qspi-nvmfs"
    0x000000200000-0x000002000000 : "qspi-linux"
    libphy: Fixed MDIO Bus: probed
    usbcore: registered new interface driver rt2500usb
    usbcore: registered new interface driver rt73usb
    usbcore: registered new interface driver rt2800usb
    usbcore: registered new interface driver rtl8187
    usbcore: registered new interface driver rtl8192cu
    usbcore: registered new interface driver rtl8xxxu
    usbcore: registered new interface driver r8152
    usbcore: registered new interface driver lan78xx
    usbcore: registered new interface driver asix
    usbcore: registered new interface driver ax88179_178a
    usbcore: registered new interface driver cdc_ether
    usbcore: registered new interface driver smsc75xx
    usbcore: registered new interface driver smsc95xx
    usbcore: registered new interface driver rndis_host
    ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    usbcore: registered new interface driver usb-storage
    usbcore: registered new interface driver usbserial
    usbcore: registered new interface driver usbserial_generic
    usbserial: USB Serial support registered for generic
    usbcore: registered new interface driver ftdi_sio
    usbserial: USB Serial support registered for FTDI USB Serial Device
    chipidea-usb2 e0002000.usb: e0002000.usb supply vbus not found, using dummy regulator
    ULPI transceiver vendor/product ID 0x0424/0x0007
    Found SMSC USB3320 ULPI transceiver.
    ULPI integrity check: passed.
    i2c /dev entries driver
    cdns-wdt f8005000.watchdog: Xilinx Watchdog Timer at e081e000 with timeout 10s
    Xilinx Zynq CpuIdle Driver started
    ledtrig-cpu: registered to indicate activity on CPUs
    hidraw: raw HID events driver (C) Jiri Kosina
    usbcore: registered new interface driver usbhid
    usbhid: USB HID core driver
    usbcore: registered new interface driver r8712u
    usbcore: registered new interface driver r8188eu
    fpga_manager fpga0: Xilinx Zynq FPGA Manager registered
    NET: Registered protocol family 17
    Registering SWP/SWPB emulation handler
    input: gpio_keys as /devices/soc0/gpio_keys/input/input0
    Freeing unused kernel memory: 1024K
    file system registered
    using random self ethernet address
    using random host ethernet address
    Mass Storage Function, version: 2009/09/11
    LUN: removable file: (no medium)
    read descriptors
    read strings
    usb0: HOST MAC 00:e0:22:b1:e0:e3
    usb0: MAC 00:05:f7:7b:a8:33
    random: crng init done
    configfs-gadget gadget: high-speed config #1: c
    #
    

    The .32 firmware seems to have been the largely same, with the noted exception of a 802.11 reg db failure and something about ratelimiting (not that I really compared the two.)

    =~=~=~=~=~=~=~=~=~=~=~= PuTTY log 2020.10.15 13:21:57 =~=~=~=~=~=~=~=~=~=~=~=
    login as: root
    root@192.168.2.1's password: 
    Welcome to:
    ______ _       _        _________________
    | ___ \ |     | |      /  ___|  _  \ ___ \
    | |_/ / |_   _| |_ ___ \ `--.| | | | |_/ /
    |  __/| | | | | __/ _ \ `--. \ | | |    /
    | |   | | |_| | || (_) /\__/ / |/ /| |\ \
    \_|   |_|\__,_|\__\___/\____/|___/ \_| \_|
    
    v0.32
    https://wiki.analog.com/university/tools/pluto
    # dmesg
    Booting Linux on physical CPU 0x0
    Linux version 4.19.0-119999-g6edc6cd (michael@mhenneri-D06) (gcc version 8.2.0 (GCC)) #319 SMP PREEMPT Mon Jul 6 15:45:01 CEST 2020
    CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
    CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
    OF: fdt: Machine model: Analog Devices PlutoSDR Rev.B (Z7010/AD9363)
    Memory policy: Data cache writealloc
    cma: Reserved 256 MiB at 0x0e400000
    On node 0 totalpages: 131072
      Normal zone: 1024 pages used for memmap
      Normal zone: 0 pages reserved
      Normal zone: 131072 pages, LIFO batch:31
    random: get_random_bytes called from start_kernel+0x7c/0x3fc with crng_init=0
    percpu: Embedded 16 pages/cpu @(ptrval) s33228 r8192 d24116 u65536
    pcpu-alloc: s33228 r8192 d24116 u65536 alloc=16*4096
    pcpu-alloc: [0] 0 [0] 1 
    Built 1 zonelists, mobility grouping on.  Total pages: 130048
    Kernel command line: console=ttyPS0,115200 maxcpus=1 rootfstype=ramfs root=/dev/ram0 rw quiet loglevel=4 uboot=U-Boot PlutoSDR v0.20-PlutoSDR-00053-g89d0754 (Jan 14 2019 - 13:15:56 +0100)
    Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
    Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
    Memory: 240952K/524288K available (6144K kernel code, 545K rwdata, 1440K rodata, 1024K init, 139K bss, 21192K reserved, 262144K cma-reserved, 0K highmem)
    Virtual kernel memory layout:
        vector  : 0xffff0000 - 0xffff1000   (   4 kB)
        fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
        vmalloc : 0xe0800000 - 0xff800000   ( 496 MB)
        lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
        pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
        modules : 0xbf000000 - 0xbfe00000   (  14 MB)
          .text : 0x(ptrval) - 0x(ptrval)   (7136 kB)
          .init : 0x(ptrval) - 0x(ptrval)   (1024 kB)
          .data : 0x(ptrval) - 0x(ptrval)   ( 546 kB)
           .bss : 0x(ptrval) - 0x(ptrval)   ( 140 kB)
    rcu: Preemptible hierarchical RCU implementation.
    rcu: 	RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
    	Tasks RCU enabled.
    rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
    NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
    efuse mapped to (ptrval)
    slcr mapped to (ptrval)
    L2C: platform modifies aux control register: 0x72360000 -> 0x72760000
    L2C: DT/platform modifies aux control register: 0x72360000 -> 0x72760000
    L2C-310 erratum 769419 enabled
    L2C-310 enabling early BRESP for Cortex-A9
    L2C-310 full line of zeros enabled for Cortex-A9
    L2C-310 ID prefetch enabled, offset 1 lines
    L2C-310 dynamic clock gating enabled, standby mode enabled
    L2C-310 cache controller enabled, 8 ways, 512 kB
    L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76760001
    zynq_clock_init: clkc starts at (ptrval)
    Zynq clock init
    sched_clock: 64 bits at 333MHz, resolution 3ns, wraps every 4398046511103ns
    clocksource: arm_global_timer: mask: 0xffffffffffffffff max_cycles: 0x4ce07af025, max_idle_ns: 440795209040 ns
    Switching to timer-based delay loop, resolution 3ns
    clocksource: ttc_clocksource: mask: 0xffff max_cycles: 0xffff, max_idle_ns: 537538477 ns
    timer #0 at (ptrval), irq=17
    Console: colour dummy device 80x30
    Calibrating delay loop (skipped), value calculated using timer frequency.. 666.66 BogoMIPS (lpj=3333333)
    pid_max: default: 32768 minimum: 301
    Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
    Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
    CPU: Testing write buffer coherency: ok
    CPU0: Spectre v2: using BPIALL workaround
    CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
    Setting up static identity map for 0x100000 - 0x100060
    rcu: Hierarchical SRCU implementation.
    smp: Bringing up secondary CPUs ...
    smp: Brought up 1 node, 1 CPU
    SMP: Total of 1 processors activated (666.66 BogoMIPS).
    CPU: All CPU(s) started in SVC mode.
    devtmpfs: initialized
    VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
    clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
    futex hash table entries: 512 (order: 3, 32768 bytes)
    pinctrl core: initialized pinctrl subsystem
    NET: Registered protocol family 16
    DMA: preallocated 256 KiB pool for atomic coherent allocations
    cpuidle: using governor ladder
    hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
    hw-breakpoint: maximum watchpoint size is 4 bytes.
    zynq-ocm f800c000.ocmc: ZYNQ OCM pool: 256 KiB @ 0x(ptrval)
    zynq-pinctrl 700.pinctrl: zynq pinctrl initialized
    e0001000.serial: ttyPS0 at MMIO 0xe0001000 (irq = 25, base_baud = 6249999) is a xuartps
    console [ttyPS0] enabled
    SCSI subsystem initialized
    usbcore: registered new interface driver usbfs
    usbcore: registered new interface driver hub
    usbcore: registered new device driver usb
    FPGA manager framework
    clocksource: Switched to clocksource arm_global_timer
    NET: Registered protocol family 2
    tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes)
    TCP established hash table entries: 4096 (order: 2, 16384 bytes)
    TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
    TCP: Hash tables configured (established 4096 bind 4096)
    UDP hash table entries: 256 (order: 1, 8192 bytes)
    UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
    NET: Registered protocol family 1
    Trying to unpack rootfs image as initramfs...
    Freeing initrd memory: 5560K
    hw perfevents: no interrupt-affinity property for /pmu@f8891000, guessing.
    hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
    Initialise system trusted keyrings
    workingset: timestamp_bits=30 max_order=17 bucket_order=0
    jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
    Key type asymmetric registered
    Asymmetric key parser 'x509' registered
    io scheduler noop registered
    io scheduler deadline registered
    io scheduler cfq registered (default)
    io scheduler mq-deadline registered
    io scheduler kyber registered
    brd: module loaded
    loop: module loaded
    m25p80 spi1.0: SPI-NOR-UniqueID 1044739659930006080031003fdc278679
    m25p80 spi1.0: n25q256a (32768 Kbytes)
    4 fixed-partitions partitions found on MTD device spi1.0
    Creating 4 MTD partitions on "spi1.0":
    0x000000000000-0x000000100000 : "qspi-fsbl-uboot"
    0x000000100000-0x000000120000 : "qspi-uboot-env"
    0x000000120000-0x000000200000 : "qspi-nvmfs"
    0x000000200000-0x000002000000 : "qspi-linux"
    libphy: Fixed MDIO Bus: probed
    usbcore: registered new interface driver rt2500usb
    usbcore: registered new interface driver rt73usb
    usbcore: registered new interface driver rt2800usb
    usbcore: registered new interface driver rtl8187
    usbcore: registered new interface driver rtl8192cu
    usbcore: registered new interface driver rtl8xxxu
    usbcore: registered new interface driver r8152
    usbcore: registered new interface driver lan78xx
    usbcore: registered new interface driver asix
    usbcore: registered new interface driver ax88179_178a
    usbcore: registered new interface driver cdc_ether
    usbcore: registered new interface driver smsc75xx
    usbcore: registered new interface driver smsc95xx
    usbcore: registered new interface driver rndis_host
    ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    usbcore: registered new interface driver usb-storage
    usbcore: registered new interface driver usbserial_generic
    usbserial: USB Serial support registered for generic
    usbcore: registered new interface driver ftdi_sio
    usbserial: USB Serial support registered for FTDI USB Serial Device
    chipidea-usb2 e0002000.usb: e0002000.usb supply vbus not found, using dummy regulator
    chipidea-usb2 e0002000.usb: Linked as a consumer to regulator.0
    ULPI transceiver vendor/product ID 0x0424/0x0007
    Found SMSC USB3320 ULPI transceiver.
    ULPI integrity check: passed.
    i2c /dev entries driver
    cdns-wdt f8005000.watchdog: Xilinx Watchdog Timer with timeout 10s
    Xilinx Zynq CpuIdle Driver started
    ledtrig-cpu: registered to indicate activity on CPUs
    hidraw: raw HID events driver (C) Jiri Kosina
    usbcore: registered new interface driver usbhid
    usbhid: USB HID core driver
    usbcore: registered new interface driver r8712u
    usbcore: registered new interface driver r8188eu
    fpga_manager fpga0: Xilinx Zynq FPGA Manager registered
    NET: Registered protocol family 17
    lib80211: common routines for IEEE802.11 drivers
    lib80211_crypt: registered algorithm 'NULL'
    lib80211_crypt: registered algorithm 'WEP'
    lib80211_crypt: registered algorithm 'CCMP'
    Registering SWP/SWPB emulation handler
    Loading compiled-in X.509 certificates
    input: gpio_keys as /devices/soc0/gpio_keys/input/input0
    cfg80211: Loading compiled-in X.509 certificates for regulatory database
    cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
    platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
    cfg80211: failed to load regulatory.db
    Freeing unused kernel memory: 1024K
    Run /init as init process
    random: fast init done
    file system registered
    using random self ethernet address
    using random host ethernet address
    Mass Storage Function, version: 2009/09/11
    LUN: removable file: (no medium)
    read descriptors
    read strings
    usb0: HOST MAC 00:e0:22:b1:e0:e3
    usb0: MAC 00:05:f7:7b:a8:33
    random: dbus-uuidgen: uninitialized urandom read (12 bytes read)
    random: dbus-uuidgen: uninitialized urandom read (8 bytes read)
    random: dbus-daemon: uninitialized urandom read (12 bytes read)
    random: crng init done
    random: 1 urandom warning(s) missed due to ratelimiting
    configfs-gadget gadget: high-speed config #1: c
    # 

  • 0
    •  Analog Employees 
    on Oct 15, 2020 11:39 PM 4 months ago in reply to wizardofwtf

    hmmm, something is strange here. It's not even trying to probe for the transceiver. Even if you physically remove the transceiver the driver will spit out something.

    Let me check in with the software team.

    -Travis

  • Are there any examples of what these logs/returns should look like?
    So there is a point at which it polls the AD9361? What interface does it use (spi,i2c) and (like i2cdetect) is there some way to manually query the device? Or is it connected directly to the logic portion (and if so, does the firmware write the bitstream each time it's updated or does it skip it if it seems to be the same version?)? Which leads me to: would trying DFU help?

    Just speculating, thanks for the help by the way.

Reply
  • Are there any examples of what these logs/returns should look like?
    So there is a point at which it polls the AD9361? What interface does it use (spi,i2c) and (like i2cdetect) is there some way to manually query the device? Or is it connected directly to the logic portion (and if so, does the firmware write the bitstream each time it's updated or does it skip it if it seems to be the same version?)? Which leads me to: would trying DFU help?

    Just speculating, thanks for the help by the way.

Children
  • +1
    •  Analog Employees 
    on Oct 16, 2020 5:59 AM 4 months ago in reply to wizardofwtf

    Did you change anything in your u-boot environment. For example used fw_setenv?

    Looks like the compatible string is set to something that isn't recognized.

    To fix this, save the entire plutosdr-fw-v0.32.zip onto the mass storage drive. Then eject and wait.

    This will also restore your u-boot environment. If this doesn't help.

    On the   mass storage drive open config.txt set 

    diagnostic_report = 1

    Save and then upload the generated diagnostic_report file here.

    -Michael

  • I errr may have attempted to extend the frequency range with the following:

    # fw_setenv attr_name compatible
    # fw_setenv attr_val ad9364

    I seem to recall there being quotes somewhere in there that don't appear on the page I
    just found, however. Now I feel dumb.

    It works! Seems to with IIO_Osc, at any rate. There are now two channels for the ad9361,
    more tabs in the other window and I get wave forms. SDRAngel is still being balky,
    but that's something else entirely.

    Thank you!