Frequency response for OP 97 Op amp using ADALM2000

Hello,

I set up a simple inverting gain Op amp circuit with the OP 97 and two resistors (100k and 10k). The circuit operates correctly with a gain of 10V/V  I measured the magnitude response using the network analyzer and i got a 3 db frequency or approximately 11 kHz.  That seems very low.  I am wondering if it is due to all of the wiring on my breadboard and the cable connections to the ADALM2000.  I am using the parts kit ADALP2000 breadboard and wires provided.

Thanks!

Parents Reply Children
No Data