Hello. I try to get an executable c program to run automatically at start from an USB stick using the OTG functionality of the Adalm Pluto. I called the file "runme0" without file extension, put in on a USB Stick and hoped that the fie will be executed automatically like shell scripts with the sh extension do without problem. I have tried to run the program directly via ssh and it ran with no problem. What shall I do to get this program to run? Is there a possibility to get an error log?
Can you post your shell script? How have you verified it's not working? Have you tried naming the script with the .sh extension?
-Travis
I have tried the following:
1. Compiled the file https://raw.githubusercontent.com/analogdevicesinc/libiio/master/examples/ad9361-iiostream.c on my windows machine. Result is the file runme0 here: (https://www.dropbox.com/s/6mrihqabml1kqby/runme0?dl=0)
2. Connect the Pluto via USB to the PC and execute the file with SSH after copiing it via SCP. This worked fine.
3. Copy the executable file to an USB stick and using the OTG functionality according to https://wiki.analog.com/university/tools/pluto/devs/usb_otg. In the standalone mode the pluto did not execute the file.
4. Copy an additional shell script to the USB stick called "runme0.sh":
#!/bin/sh
cd /media/sda1/
chmod +x runme0
./runme0
5. The script has been executed in standalone mode but the executable file "runme0" did not start. At least the shell script has been executed as I have added some additional commands but the pluto did not start the compiled file "runme0".
Does anyone know what went wrong? Is there a possibility to log the command line error Messages into a file on the USB stick as this would help a lot for Debugging?
Thanks,
Hanno
Please do not name the executable runme0, as the autorun script might get confused. Naming the shell script runme0.sh is fine.
I would not directly use that example since it has no end or stop point.
-Travis
I have tried to rename the executable but it still did not work. Is there a reason why the program does not run directly via OTG? Do you have another example that proves the concept of executing programs via OTG?
I have tried to rename the executable but it still did not work. Is there a reason why the program does not run directly via OTG? Do you have another example that proves the concept of executing programs via OTG?
I changed the c example to run for only a few iterations of the loop and it worked fine.
Here is the runme0.sh script:
#!/bin/sh # the default directory the script runs in is /dev, so change to the drive cd /media/sda1/ # create a file touch foobar.txt echo default-on > /sys/class/leds/led0:green/trigger >> foobar.txt sleep 3 chmod +x pluto_stream ./pluto_stream >> foobar.txt echo none > /sys/class/leds/led0:green/trigger >> foobar.txt # Set the LO up /usr/bin/iio_attr -a -c ad9361-phy TX_LO frequency 908460000 >> foobar.txt # Set the Sample frequency up, tone will appear at sampling_frequency/32 /usr/bin/iio_attr -a -c -o ad9361-phy voltage0 sampling_frequency 32000000 >> foobar.txt # Turn the attenuation down /usr/bin/iio_attr -a -c -o ad9361-phy voltage0 hardwaregain 0 # https://wiki.analog.com/resources/tools-software/linux-drivers/iio-transceiver/ad9361#bist_tone # Inject 0dBFS tone at Fsample/32 into TX (all channels enabled) /usr/bin/iio_attr -a -D ad9361-phy bist_tone "1 0 0 0" >> foobar.txt cd /root ACTION=remove_all /lib/mdev/automounter.sh
Here is the modified c example:
/* * libiio - AD9361 IIO streaming example * * Copyright (C) 2014 IABG mbH * Author: Michael Feilen <feilen_at_iabg.de> * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License * as published by the Free Software Foundation; either version 2 * of the License, or (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 51 Franklin Street, Fifth Floor, Boston, MA 02110-1301, USA. **/ #include <stdbool.h> #include <stdint.h> #include <string.h> #include <signal.h> #include <stdio.h> #ifdef __APPLE__ #include <iio/iio.h> #else #include <iio.h> #endif /* helper macros */ #define MHZ(x) ((long long)(x*1000000.0 + .5)) #define GHZ(x) ((long long)(x*1000000000.0 + .5)) #define IIO_ENSURE(expr) { \ if (!(expr)) { \ (void) fprintf(stderr, "assertion failed (%s:%d)\n", __FILE__, __LINE__); \ (void) abort(); \ } \ } /* RX is input, TX is output */ enum iodev { RX, TX }; /* common RX and TX streaming params */ struct stream_cfg { long long bw_hz; // Analog banwidth in Hz long long fs_hz; // Baseband sample rate in Hz long long lo_hz; // Local oscillator frequency in Hz const char* rfport; // Port name }; /* static scratch mem for strings */ static char tmpstr[64]; /* IIO structs required for streaming */ static struct iio_context *ctx = NULL; static struct iio_channel *rx0_i = NULL; static struct iio_channel *rx0_q = NULL; static struct iio_channel *tx0_i = NULL; static struct iio_channel *tx0_q = NULL; static struct iio_buffer *rxbuf = NULL; static struct iio_buffer *txbuf = NULL; static bool stop; /* cleanup and exit */ static void shutdown() { printf("* Destroying buffers\n"); if (rxbuf) { iio_buffer_destroy(rxbuf); } if (txbuf) { iio_buffer_destroy(txbuf); } printf("* Disabling streaming channels\n"); if (rx0_i) { iio_channel_disable(rx0_i); } if (rx0_q) { iio_channel_disable(rx0_q); } if (tx0_i) { iio_channel_disable(tx0_i); } if (tx0_q) { iio_channel_disable(tx0_q); } printf("* Destroying context\n"); if (ctx) { iio_context_destroy(ctx); } exit(0); } static void handle_sig(int sig) { printf("Waiting for process to finish... Got signal %d\n", sig); stop = true; } /* check return value of attr_write function */ static void errchk(int v, const char* what) { if (v < 0) { fprintf(stderr, "Error %d writing to channel \"%s\"\nvalue may not be supported.\n", v, what); shutdown(); } } /* write attribute: long long int */ static void wr_ch_lli(struct iio_channel *chn, const char* what, long long val) { errchk(iio_channel_attr_write_longlong(chn, what, val), what); } /* write attribute: string */ static void wr_ch_str(struct iio_channel *chn, const char* what, const char* str) { errchk(iio_channel_attr_write(chn, what, str), what); } /* helper function generating channel names */ static char* get_ch_name(const char* type, int id) { snprintf(tmpstr, sizeof(tmpstr), "%s%d", type, id); return tmpstr; } /* returns ad9361 phy device */ static struct iio_device* get_ad9361_phy(struct iio_context *ctx) { struct iio_device *dev = iio_context_find_device(ctx, "ad9361-phy"); IIO_ENSURE(dev && "No ad9361-phy found"); return dev; } /* finds AD9361 streaming IIO devices */ static bool get_ad9361_stream_dev(struct iio_context *ctx, enum iodev d, struct iio_device **dev) { switch (d) { case TX: *dev = iio_context_find_device(ctx, "cf-ad9361-dds-core-lpc"); return *dev != NULL; case RX: *dev = iio_context_find_device(ctx, "cf-ad9361-lpc"); return *dev != NULL; default: IIO_ENSURE(0); return false; } } /* finds AD9361 streaming IIO channels */ static bool get_ad9361_stream_ch(__notused struct iio_context *ctx, enum iodev d, struct iio_device *dev, int chid, struct iio_channel **chn) { *chn = iio_device_find_channel(dev, get_ch_name("voltage", chid), d == TX); if (!*chn) *chn = iio_device_find_channel(dev, get_ch_name("altvoltage", chid), d == TX); return *chn != NULL; } /* finds AD9361 phy IIO configuration channel with id chid */ static bool get_phy_chan(struct iio_context *ctx, enum iodev d, int chid, struct iio_channel **chn) { switch (d) { case RX: *chn = iio_device_find_channel(get_ad9361_phy(ctx), get_ch_name("voltage", chid), false); return *chn != NULL; case TX: *chn = iio_device_find_channel(get_ad9361_phy(ctx), get_ch_name("voltage", chid), true); return *chn != NULL; default: IIO_ENSURE(0); return false; } } /* finds AD9361 local oscillator IIO configuration channels */ static bool get_lo_chan(struct iio_context *ctx, enum iodev d, struct iio_channel **chn) { switch (d) { // LO chan is always output, i.e. true case RX: *chn = iio_device_find_channel(get_ad9361_phy(ctx), get_ch_name("altvoltage", 0), true); return *chn != NULL; case TX: *chn = iio_device_find_channel(get_ad9361_phy(ctx), get_ch_name("altvoltage", 1), true); return *chn != NULL; default: IIO_ENSURE(0); return false; } } /* applies streaming configuration through IIO */ bool cfg_ad9361_streaming_ch(struct iio_context *ctx, struct stream_cfg *cfg, enum iodev type, int chid) { struct iio_channel *chn = NULL; // Configure phy and lo channels printf("* Acquiring AD9361 phy channel %d\n", chid); if (!get_phy_chan(ctx, type, chid, &chn)) { return false; } wr_ch_str(chn, "rf_port_select", cfg->rfport); wr_ch_lli(chn, "rf_bandwidth", cfg->bw_hz); wr_ch_lli(chn, "sampling_frequency", cfg->fs_hz); // Configure LO channel printf("* Acquiring AD9361 %s lo channel\n", type == TX ? "TX" : "RX"); if (!get_lo_chan(ctx, type, &chn)) { return false; } wr_ch_lli(chn, "frequency", cfg->lo_hz); return true; } /* simple configuration and streaming */ /* usage: * Default context, assuming local IIO devices, i.e., this script is run on ADALM-Pluto for example $./a.out * URI context, find out the uri by typing `iio_info -s` at the command line of the host PC $./a.out usb:x.x.x */ int main (int argc, char **argv) { // Streaming devices struct iio_device *tx; struct iio_device *rx; // RX and TX sample counters size_t nrx = 0; size_t ntx = 0; // Stream configurations struct stream_cfg rxcfg; struct stream_cfg txcfg; // Listen to ctrl+c and IIO_ENSURE signal(SIGINT, handle_sig); // RX stream config rxcfg.bw_hz = MHZ(2); // 2 MHz rf bandwidth rxcfg.fs_hz = MHZ(2.5); // 2.5 MS/s rx sample rate rxcfg.lo_hz = GHZ(2.5); // 2.5 GHz rf frequency rxcfg.rfport = "A_BALANCED"; // port A (select for rf freq.) // TX stream config txcfg.bw_hz = MHZ(1.5); // 1.5 MHz rf bandwidth txcfg.fs_hz = MHZ(2.5); // 2.5 MS/s tx sample rate txcfg.lo_hz = GHZ(2.5); // 2.5 GHz rf frequency txcfg.rfport = "A"; // port A (select for rf freq.) printf("* Acquiring IIO context\n"); if (argc == 1) { IIO_ENSURE((ctx = iio_create_default_context()) && "No context"); } else if (argc == 2) { IIO_ENSURE((ctx = iio_create_context_from_uri(argv[1])) && "No context"); } IIO_ENSURE(iio_context_get_devices_count(ctx) > 0 && "No devices"); printf("* Acquiring AD9361 streaming devices\n"); IIO_ENSURE(get_ad9361_stream_dev(ctx, TX, &tx) && "No tx dev found"); IIO_ENSURE(get_ad9361_stream_dev(ctx, RX, &rx) && "No rx dev found"); printf("* Configuring AD9361 for streaming\n"); IIO_ENSURE(cfg_ad9361_streaming_ch(ctx, &rxcfg, RX, 0) && "RX port 0 not found"); IIO_ENSURE(cfg_ad9361_streaming_ch(ctx, &txcfg, TX, 0) && "TX port 0 not found"); printf("* Initializing AD9361 IIO streaming channels\n"); IIO_ENSURE(get_ad9361_stream_ch(ctx, RX, rx, 0, &rx0_i) && "RX chan i not found"); IIO_ENSURE(get_ad9361_stream_ch(ctx, RX, rx, 1, &rx0_q) && "RX chan q not found"); IIO_ENSURE(get_ad9361_stream_ch(ctx, TX, tx, 0, &tx0_i) && "TX chan i not found"); IIO_ENSURE(get_ad9361_stream_ch(ctx, TX, tx, 1, &tx0_q) && "TX chan q not found"); printf("* Enabling IIO streaming channels\n"); iio_channel_enable(rx0_i); iio_channel_enable(rx0_q); iio_channel_enable(tx0_i); iio_channel_enable(tx0_q); printf("* Creating non-cyclic IIO buffers with 1 MiS\n"); rxbuf = iio_device_create_buffer(rx, 1024*1024, false); if (!rxbuf) { perror("Could not create RX buffer"); shutdown(); } txbuf = iio_device_create_buffer(tx, 1024*1024, false); if (!txbuf) { perror("Could not create TX buffer"); shutdown(); } printf("* Starting IO streaming (press CTRL+C to cancel)\n"); int count = 0; while (!stop) { count++; if (count>=20) break; ssize_t nbytes_rx, nbytes_tx; char *p_dat, *p_end; ptrdiff_t p_inc; // Schedule TX buffer nbytes_tx = iio_buffer_push(txbuf); if (nbytes_tx < 0) { printf("Error pushing buf %d\n", (int) nbytes_tx); shutdown(); } // Refill RX buffer nbytes_rx = iio_buffer_refill(rxbuf); if (nbytes_rx < 0) { printf("Error refilling buf %d\n",(int) nbytes_rx); shutdown(); } // READ: Get pointers to RX buf and read IQ from RX buf port 0 p_inc = iio_buffer_step(rxbuf); p_end = iio_buffer_end(rxbuf); for (p_dat = (char *)iio_buffer_first(rxbuf, rx0_i); p_dat < p_end; p_dat += p_inc) { // Example: swap I and Q const int16_t i = ((int16_t*)p_dat)[0]; // Real (I) const int16_t q = ((int16_t*)p_dat)[1]; // Imag (Q) ((int16_t*)p_dat)[0] = q; ((int16_t*)p_dat)[1] = i; } // WRITE: Get pointers to TX buf and write IQ to TX buf port 0 p_inc = iio_buffer_step(txbuf); p_end = iio_buffer_end(txbuf); for (p_dat = (char *)iio_buffer_first(txbuf, tx0_i); p_dat < p_end; p_dat += p_inc) { // Example: fill with zeros // 12-bit sample needs to be MSB alligned so shift by 4 // https://wiki.analog.com/resources/eval/user-guides/ad-fmcomms2-ebz/software/basic_iq_datafiles#binary_format ((int16_t*)p_dat)[0] = 0 << 4; // Real (I) ((int16_t*)p_dat)[1] = 0 << 4; // Imag (Q) } // Sample counter increment and status output nrx += nbytes_rx / iio_device_get_sample_size(rx); ntx += nbytes_tx / iio_device_get_sample_size(tx); printf("\tRX %8.2f MSmp, TX %8.2f MSmp\n", nrx/1e6, ntx/1e6); } shutdown(); return 0; }
Here is the output I get in OTG:
default-on Using auto-detected IIO context at URI "local:" dev 'ad9361-phy', channel 'altvoltage1' (output), id 'TX_LO', attr 'frequency', value '2450000000' wrote 10 bytes to frequency dev 'ad9361-phy', channel 'altvoltage1' (output), id 'TX_LO', attr 'frequency', value '908460000' Using auto-detected IIO context at URI "local:" dev 'ad9361-phy', channel 'voltage0' (output), attr 'sampling_frequency', value '30720000' wrote 9 bytes to sampling_frequency dev 'ad9361-phy', channel 'voltage0' (output), attr 'sampling_frequency', value '32000000' Using auto-detected IIO context at URI "local:" dev 'ad9361-phy', debug attr 'bist_tone', value :'0' wrote 8 bytes to bist_tone dev 'ad9361-phy', debug attr 'bist_tone', value :'1' default-on default-on * Acquiring IIO context * Acquiring AD9361 streaming devices * Configuring AD9361 for streaming * Acquiring AD9361 phy channel 0 * Acquiring AD9361 RX lo channel * Acquiring AD9361 phy channel 0 * Acquiring AD9361 TX lo channel * Initializing AD9361 IIO streaming channels * Enabling IIO streaming channels * Creating non-cyclic IIO buffers with 1 MiS * Starting IO streaming (press CTRL+C to cancel) RX 1.05 MSmp, TX 1.05 MSmp RX 2.10 MSmp, TX 2.10 MSmp RX 3.15 MSmp, TX 3.15 MSmp RX 4.19 MSmp, TX 4.19 MSmp RX 5.24 MSmp, TX 5.24 MSmp RX 6.29 MSmp, TX 6.29 MSmp RX 7.34 MSmp, TX 7.34 MSmp RX 8.39 MSmp, TX 8.39 MSmp RX 9.44 MSmp, TX 9.44 MSmp RX 10.49 MSmp, TX 10.49 MSmp RX 11.53 MSmp, TX 11.53 MSmp RX 12.58 MSmp, TX 12.58 MSmp RX 13.63 MSmp, TX 13.63 MSmp RX 14.68 MSmp, TX 14.68 MSmp RX 15.73 MSmp, TX 15.73 MSmp RX 16.78 MSmp, TX 16.78 MSmp RX 17.83 MSmp, TX 17.83 MSmp RX 18.87 MSmp, TX 18.87 MSmp RX 19.92 MSmp, TX 19.92 MSmp * Destroying buffers * Disabling streaming channels * Destroying context none Using auto-detected IIO context at URI "local:" dev 'ad9361-phy', channel 'altvoltage1' (output), id 'TX_LO', attr 'frequency', value '2500000000' wrote 10 bytes to frequency dev 'ad9361-phy', channel 'altvoltage1' (output), id 'TX_LO', attr 'frequency', value '908460000' Using auto-detected IIO context at URI "local:" dev 'ad9361-phy', channel 'voltage0' (output), attr 'sampling_frequency', value '2500000' wrote 9 bytes to sampling_frequency dev 'ad9361-phy', channel 'voltage0' (output), attr 'sampling_frequency', value '32000000' Using auto-detected IIO context at URI "local:" dev 'ad9361-phy', debug attr 'bist_tone', value :'0' wrote 8 bytes to bist_tone dev 'ad9361-phy', debug attr 'bist_tone', value :'1'
-Travis
Your example stil does not work. The test tone commands in your runme0.sh file lead to a transmit signal but before the "pluto_stream" program should start. This is not the case. On the other Hand, where do you get the OTG Output? Do you find it on the USB drive after execution? I can not find any file. I will describe now exactly the steps I do so you may see, where the Problem lies:
1. The preparation of the data is done on my Windows10 machine.
2. I copy the content of your "runme0.sh" example to a Textfile with the Name "runme0.sh" and write it to a clean 2 GB USB Drive with FAT32 file Format.
3. I copy the Content of your c example Code above in a Textfile called "pluto_stream.c".
4. Using the Compiler "gcc-arm-9.2-2019.12-mingw-w64-i686-arm-none-linux-gnueabihf" and the Sysroot v0.31 (same Version as in the Pluto) I perform the compilation from the Folder the c file is put to with following command:
arm-none-linux-gnueabihf-gcc -mfloat-abi=hard --sysroot=C:\Users\hanno_000\Documents\Amateurfunk\Pluto\sysroot-v0.31.tar\staging -std=gnu99 -g -o pluto_stream pluto_stream.c -lpthread -liio -lm -Wall -Wextra
5. I copy the Output file "pluto_stream" to the USB drive.
6. The Pluto is supplied via the Right Mini USB Input.
7. I insert the USB drive to the Pluto.
8. The blinking frequency changes for a short period then goes back to the normal Flash interval.
9. Check if signals are on the Air.
10. Remove USB drive, put it to the PC, there is no additional log file on it.
I have to say that the reason why I believe that the executable file is not started is because I made an Experiment by commenting out the test tone and modified your c source Code just to get a sine Signal at 144.9MHz to see if it works. The program itself runs as expected directly via ssh but still not standalone. When I then activate your test tone commands in the "runme0.sh" script (changing the transmit frequency to 144.9MHz) the signal is sent.
So still the same Problem, the script runs but the c program not. Do you have an idea?
So if no log file is created then the script isn't running, the USB isn't writable, or the script has some encoding which Pluto cannot interpret.
Here is my generated executable https://wiki.analog.com/_media/university/tools/pluto_stream_rename.doc (rename to pluto_stream)
-Travis
Hello Travis,
I tried your executable after renaming it correctly. The program still does not execute and the file is not generated. The rest of the script is running so I am now Looking towards the write Access of the USB stick. This may explain why the executable is not running because the "chmod" command could be rejected and the executable therefore is not startable.
I tried with 2 USB Sticks now but no success. Did you use FAT or another filesystem? Do you format your drive with Linux or windows? Maybe there are differences.
sdf └─sdf1 vfat TEST 4017-B37F /media/tcollins/TEST sdg └─sdg1 vfat PlutoSDR F6F3-FAA0 /media/tcollins/PlutoSDR
Everything is done in Linux from my side.
-Travis
Hi Travis,
I have tried now to check if the USB drive is writable under Linux using my RaspberryPi4. After plugging the USB drive in a free Slot the USB drive was automatically mounted as expected and read and write Access was granted.
Then I unmounted the Drive manually and remount it again with the procedure in the automounter.sh script on the pluto:
1. mkdir -p "/media/sda1"
2. mount -t auto -o sync "/dev/sda1" "/media/sda1"
After this Manual mounting I had no permission to write to the USB drive anymore. So I think the same happens on the Pluto. I do not know what the difference is between the automounter on the raspian and the manual mounting but at this Point there seems to be the Problem. Also after trying to Change the Access rights with "chown" or "chmod" did not succeed in the Manual mounting mode. Maybe you have an idea.
I would suggest formatting on a Linux system if you can. Maybe Windows is doing something strange.
-Travis
The executable works now and also the log file is generated. It had Nothing to do with the USB drive, it was the script file that was generated with on Windows. I opened the file with a Linux System, copied the content to a new text file generated in Linux. That was it. There has been a hint on the OTG page around here saying to insert 'LF' at the end of the line using Windows, I think it had something to do with it.
Hi Hanno,
Could you please share the script of your runme0.sh
with me? I am trying to achieve the same task of copying pluto_stream.txt
to a desired location on PlutoSDR, but I haven't been successful so far. It would be incredibly helpful if you could share your script.
Thanks a lot!
Hey, I figured it out. There was a directory mistake. Thanks!