Post Go back to editing

Bricked ADALM-PLUTO

someone on twitter asked:

Just got my PlutoSDR, tried updating the firmware to 0.31, bricked it.
Ran dfu-util to unbrick it, says it's done but it's still bricked. Any clues?
LED1 is solid, ready LED is off.
Output from update.bat:
Opening DFU capable USB device...
ID 0456:b674
Run-time device DFU version 0110
Claiming USB DFU Interface...
Setting Alternate Setting #1 ...
Determining device status: state = dfuIDLE, status = 0
dfuIDLE, continuing
DFU mode device DFU version 0110
Device returned transfer size 4096
Copying data from PC to DFU device
Download        [=========================] 100%     10100803 bytes
Download done.
state(7) = dfuMANIFEST, status(0) = No error condition is present
state(2) = dfuIDLE, status(0) = No error condition is present
Done!
Parents Reply Children
No Data