someone on twitter asked:
Just got my PlutoSDR, tried updating the firmware to 0.31, bricked it. Ran dfu-util to unbrick it, says it's done but it's still bricked. Any clues? LED1 is solid, ready LED is off. Output from update.bat: Opening DFU capable USB device... ID 0456:b674 Run-time device DFU version 0110 Claiming USB DFU Interface... Setting Alternate Setting #1 ... Determining device status: state = dfuIDLE, status = 0 dfuIDLE, continuing DFU mode device DFU version 0110 Device returned transfer size 4096 Copying data from PC to DFU device Download [=========================] 100% 10100803 bytes Download done. state(7) = dfuMANIFEST, status(0) = No error condition is present state(2) = dfuIDLE, status(0) = No error condition is present Done!