Pluto SDR showing only 2 devices

I received my PlutoSDR in the mail, and started setting it up on an Ubuntu 16.04 machine today. I've gone through the process of compiling libiio, gr-iio, libad9361-iio, and iio-oscilloscope. When I run the 'iio_info -a' or 'iio_info -u ip:192.168.2.1', the results show only 2 devices listed - 'adm1177' and 'xadc', In all of the online tutorials I've seen, there are 5 devices. When I use the oscilloscope program, it's not seeing them either. I seem to be missing the ad9361-phy, cf-ad9361-dds-core-lpc, and cf-ad9361-lpc devices.

I have updated the firmware pluto.frm and also updated using the dfu-util, but the devices are still missing. Am I doing something wrong here? I cannot get the scope to work, nor the device to connect in GNURadio. 

I have a Rev B board.

Thanks,

-Steve

Top Replies

    •  Analog Employees 
    Feb 15, 2019 in reply to Pacmanfan321 +1 verified
    ad9361-phy,model:

    Looks like you played with the fw_setenv commands and erased the compatible name completely.

    Please do whatever you did again, and properly set the name.

    -Michael