ADALM-PLUTO not detected on Windows 10

Pluto was working nicely on Windows 10 with latest firmware and driver (0.7). Next I installed the Matlab Communication Thing to use it from Matlab. The component installed - again - the driver and when I clicked on the configure button device was not found. I re-plugged the device and nothing happened - like I did not plug anything into the PC - even used usbview from debug tools to check and it shows nothing was plugged. I tried different USB ports with the same result. All ports work fine if I plug something else into them (tried both USB 2 and 3 devices). If I plug the PLUTO into other computer it will work correctly (ie shows up as mass storage). On the PLUTO the Ready LED is on and LED1 is blinking after plugin in.

I reinstalled the driver about 10 times. Tried to uninstall it, also uninstalled all the hidden devices manually in device manager, all without success.

Any idea what could be wrong and what I can do about it?

Parents
  • +1
    •  Analog Employees 
    on Aug 20, 2018 10:07 PM over 1 year ago

    Also have you tried rebooting?

    -Travis

  • 0
    •  Analog Employees 
    on Jul 14, 2020 8:49 PM 20 days ago in reply to travisfcollins

    Hi

    I have the similar situation where my pluto is not detected in windows but working in linux.

    I have two Plutos, Pluto1 and Pluto2.

    • Pluto 1:
      • The Windows Problem Pluto. It is detected in WIndows 10 only under "libusb-win32 devices" as "PlutoSDRDA". Not detected as Mass storage device neither serial port or any other adapter in Windows.
      • It is not detected by MAtlab as well.
      • If i connect it to Linux(Ubuntu). It is working fine. I have tested with Libiio commands and all working.
    • Pluto 2:
      • The Windows working pluto. It is working fine with Windows 10. It appears as Mass Storage device and I can connect it using Matlab and run the examples on Matlab. I dont have Libiio installed in Windows.

    Any help.

    Thanks

    IK

Reply
  • 0
    •  Analog Employees 
    on Jul 14, 2020 8:49 PM 20 days ago in reply to travisfcollins

    Hi

    I have the similar situation where my pluto is not detected in windows but working in linux.

    I have two Plutos, Pluto1 and Pluto2.

    • Pluto 1:
      • The Windows Problem Pluto. It is detected in WIndows 10 only under "libusb-win32 devices" as "PlutoSDRDA". Not detected as Mass storage device neither serial port or any other adapter in Windows.
      • It is not detected by MAtlab as well.
      • If i connect it to Linux(Ubuntu). It is working fine. I have tested with Libiio commands and all working.
    • Pluto 2:
      • The Windows working pluto. It is working fine with Windows 10. It appears as Mass Storage device and I can connect it using Matlab and run the examples on Matlab. I dont have Libiio installed in Windows.

    Any help.

    Thanks

    IK

Children
No Data