ADAU1452 Basic Starter Project

This video shows how to start a project from scratch and talks about some of the details of this processor. The video walks you though setting up a basic project that has inputs, outputs, a test oscillator and some meters. This is a great "starter" project to keep in your folder to use when you need to start a new project. It has all the basic elements needed for starting a new project. It was developed for the EVAL-ADAU1452MINIZ or the EVAL-ADAU1452RevBZ evaluation boards. It will also work for the EVAL-ADAU1466RevBZ board.

Link to SigmaStudio project files: https://ez.analog.com/dsp/sigmadsp/m/file-uploads/3238

  • Once you’re comfortable with this baseline, it becomes much easier to experiment without fear of breaking everything. You can drop in filters, compressors, or routing changes and immediately see how they affect levels and behavior. That feedback loop is huge when you’re learning SigmaStudio’s quirks. It also reinforces good habits early, like checking headroom and watching meters instead of guessing. For teaching or onboarding new team members, this kind of project is gold. It lowers the barrier to entry and builds confidence fast. From there, scaling up to more complex website designs feels far less intimidating.

  • This is a really solid starting point if you’re new to the ADAU1452 or SigmaStudio in general. The project shown is simple, but that’s the whole value. You get inputs, outputs, a test tone, and meters already wired up, so you’re not staring at a blank canvas. It helps you focus on learning signal flow and processor basics instead of setup headaches. Keeping something like this saved is smart, because you can reuse it every time you start a new design. It also makes it easier to debug later, since you know the foundation already works. For anyone using the 1452 or even the 1466 eval boards, this kind of template saves a lot of time and frustration.