Post Go back to editing

lib-iio and gr-iio instalation error with pybombs

hi,

I'm getting this error trying to install the libiio and gr-iio with pyboms (with command sudo pybombs install gr-iio):

[  4%] Building C object CMakeFiles/iio.dir/serial.c.o
/home/julian/prefix/src/libiio/serial.c: In function ‘serial_read_data’:
/home/julian/prefix/src/libiio/serial.c:204:49: warning: implicit declaration of function ‘sp_blocking_read_next’ [-Wimplicit-function-declaration]
  ssize_t ret = (ssize_t) libserialport_to_errno(sp_blocking_read_next(
                                                 ^
/home/julian/prefix/src/libiio/serial.c: In function ‘serial_create_context’:
/home/julian/prefix/src/libiio/serial.c:334:45: error: ‘SP_MODE_READ_WRITE’ undeclared (first use in this function)
  ret = libserialport_to_errno(sp_open(port, SP_MODE_READ_WRITE));
                                             ^
/home/julian/prefix/src/libiio/serial.c:334:45: note: each undeclared identifier is reported only once for each function it appears in
/home/julian/prefix/src/libiio/serial.c:350:9: warning: implicit declaration of function ‘sp_get_port_description’ [-Wimplicit-function-declaration]
  desc = sp_get_port_description(port);
         ^
/home/julian/prefix/src/libiio/serial.c:350:7: warning: assignment makes pointer from integer without a cast [-Wint-conversion]
  desc = sp_get_port_description(port);
       ^
CMakeFiles/iio.dir/build.make:254: recipe for target 'CMakeFiles/iio.dir/serial.c.o' failed
make[2]: *** [CMakeFiles/iio.dir/serial.c.o] Error 1
CMakeFiles/Makefile2:67: recipe for target 'CMakeFiles/iio.dir/all' failed
make[1]: *** [CMakeFiles/iio.dir/all] Error 2
Makefile:127: recipe for target 'all' failed
make: *** [all] Error 2
    PyBOMBS.Packager.source - ERROR - Build failed. See output above for error messages.
PyBOMBS.Packager.source - ERROR - Problem occurred while building package libiio:
Build failed.
PyBOMBS.install_manager - ERROR - Error installing package libiio. Aborting.

It seems an error related with serial port but I don't knopw how to solve.

Regards.

Parents Reply Children
No Data