Post Go back to editing

I would appreciate it if you could help me solve the Adalm-Pluto connection problem. I am a ham radio operator. When I use the internet browser with the IP address 192.168.2.1, I can connect to the Pluto. When I try to connect to another program, such as D

Thread Summary

The user experiences connection issues with an Analog Devices Pluto SDR AD9363 when using programs like DATV-red or SDRConsole, despite successful browser connections via IP address 192.168.2.1. The final answer suggests performing a firmware update, with a link to the official guide provided. The accompanying answer reiterates the firmware update recommendation.
AI Generated Content
Category: Hardware

I would appreciate it if you could help me solve the Adalm-Pluto connection problem. I am a ham radio operator. When I use the internet browser with the IP address 192.168.2.1, I can connect to the Pluto. When I try to connect to another program, such as DATV-red or SDRConsole, it fails to communicate data and does not recognize the Analog Devices Pluto SDR AD9363. I have another identical Pluto with the same configuration that works perfectly and connects to all programs. I have tried everything possible and cannot get it to work. Thank you.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.