Post Go back to editing

Figure 8 Transformer DC-DC booster delivers 1 mA at 15 V.

Thread Summary

The user inquires about the pin configuration for the HPH1-1400L Hexapath transformer in a 1:5 step-up configuration for use with the YX8018 part. The final answer directs the user to refer to the pinout in Figure 3 of the Analog Devices lab on bipolar step-up DC-DC converters. The step-up transformer may have been salvaged from a Dollar store burglar alarm.
AI Generated Content
Category: Hardware
Product Number: Coilcraft Hexapath 6 winding HPH1-1400L

in this lab: https://wiki.analog.com/university/courses/alm1k/alm-lab-15

The hexapath is configured as a 1:5 step up transformer. I have the breakout board version of this transformer from the ADALP2000 parts kit. Can someone please tell me what pin numbers are involved 1) when connecting the YX8018 part to one side of the transformer and 2) what pin numbers are connected to the step up side going to the load? Also, do any pins have to be linked?

Thanking you in advance.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.