Post Go back to editing

Latest Revision sends user to version 2.1.0 which doesn't work (Easy Fix)

Category: Software
Product Number: ADALM2000/Scopy
Software Version: SCOPY V1.5.0R1

Scopy "ABOUT/LATEST RELEASE" sends you to Version 2.1.0.     The current supported Release is Version 1.5.0 R1.    Unfortunately Version 2.1.0 has significant bugs.    All that needs to be fixed is the link so it points to the official SCOPY download page which is currently 1.5.0R1.

I am an instructor for ENGR202 at Oregon State University.     I have installation instructions that sends students to the correct installation page.     However, a few found the "Latest Release" on the about page.    This caused a couple of days of frustration and lost work as V2.1.0 has significant bugs (Basically it doesn't work).    As this is a simple change of link I am hopeful that you can address it.

Thank Ed

Parents
  • Well that is interesting.     I also have a Dell Laptop running Windows 11.    When running Ver 2.1.0 -r2, which is what you get from "Get Latest Release", the M2k Icon has a red "x" in the lower corner.    When you connect to the device is spends quite a bit of time in the calibration process and crashes.

    I have two students that accidently found there way to V2.1 and they both had the same experience.     One was on a MAC and the other on a Windows 11 box.

    The official Scopy Download Site is hosting V1.5.0 R1 which is what my class has been using for the last two terms without problem.    As AD is not hosting V2.1 on the official download site I figure they are aware of the bugs in V2.1.     At least that is a rational reason for continuing to present V1.5 on the official site.

    I have not reported the problem on GitHub, but will do so.

    Thanks Ed

Reply
  • Well that is interesting.     I also have a Dell Laptop running Windows 11.    When running Ver 2.1.0 -r2, which is what you get from "Get Latest Release", the M2k Icon has a red "x" in the lower corner.    When you connect to the device is spends quite a bit of time in the calibration process and crashes.

    I have two students that accidently found there way to V2.1 and they both had the same experience.     One was on a MAC and the other on a Windows 11 box.

    The official Scopy Download Site is hosting V1.5.0 R1 which is what my class has been using for the last two terms without problem.    As AD is not hosting V2.1 on the official download site I figure they are aware of the bugs in V2.1.     At least that is a rational reason for continuing to present V1.5 on the official site.

    I have not reported the problem on GitHub, but will do so.

    Thanks Ed

Children
No Data