Post Go back to editing

UNABLE TO ADALM PLUTO AS LFM RADAR

Thread Summary

The user experienced issues with LFM radar experiments using PlutoSDR in GNU Radio, including missing or inaccurate RX signals due to improper signal scaling, high TX attenuation, and unsuitable RX gain settings. The final answer suggests that 6 MSPS exceeds the USB2 interface rate, causing data bursts with gaps, and that connected graphs with two rate pacing blocks can cause contention. The solution recommends using cyclic mode with disconnected graphs to improve performance.
AI Generated Content
Category: Hardware

While performing LFM radar experiments using PlutoSDR in GNU Radio, a 10 m RF cable was used as a direct TX–RX loopback for testing. However, the received signal was not always visible, and sometimes no RX signal was obtained at all. Even when the signal was received, the processed data did not produce the correct beat frequency corresponding to the 10 m range, which resulted in inaccurate range estimation. These issues were mainly due to improper signal scaling, high TX attenuation, and unsuitable RX gain settings in the PlutoSDR configuration.

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.