Post Go back to editing

ADALM-PHASER CN0566 Python Calibration

Thread Summary

The user encountered issues with the phase sweep plot not matching the desired plot from the CN0566 Calibration page while running the phaser_examples.py script. The problem was resolved by ensuring the HB100 was correctly oriented. For similar issues, lowering the max VCO frequency in the config.py file and using a USB C power supply rated at 3.5A or 4.0A are recommended.
AI Generated Content
Category: Hardware

When attempting to run the phaser_examples.py cal file, I am unable to get a phase sweep plot that matches the desired plot from the CN0566 Calibration page on the wiki as apart of lab 1. 


the phase sweep plot obtained after calibration

the final result using phaser_gui.py


the phaser is directly inline with the hb100, verfied by laser level.